Skip to content
Siemens Developer Portal

mdsp spectrum-analysis Command

Syntax:

mdsp spectrum-analysis

Help:

mdsp spectrum-analysis --help

Alternative form:

mc spectrum-analysis

(The CLI was using mc as default command name in older versions)

Description

perform spectrum analysis on a sound file @

Usage

Parameter list:

Usage: mdsp spectrum-analysis|sp [options]

perform spectrum analysis on a sound file @

Options:
 -f, --file wav file to upload or json to analyze (default for threshold detection:
 fft.spectrum.json)
 -m, --mode [fft|threshold] Fast Fourier Transformation or threshold detection (default: "fft")
 -t, --thresholds threshold json for threshold detection (default: "thresholds.spectrum.json")
 -t, --output output file (fft: fft.spectrum.json, threshold:
 violations.spectrum.json)
 -w, --windowtype [flattop|hamming|hanning|blackman] window type for the FFT (default: "flattop")
 -y, --retry retry attempts before giving up (default: "3")
 -p, --passkey passkey
 -v, --verbose verbose output
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp spectrum-analysis command:

 Examples:

 mdsp spectrum-analysis -f machine.wav Decomposes the sound file into frequency components
 mdsp spectrum-analysis -f machine.wav --windowtype blackman use blackman window type for FFT preprocessing
 mdsp spectrum-analysis --mode threshold detect threshold violations for thresholds stored in thresholds.spectrum.json

See Insights Hub API documentation for more information about Insights Hub APIs.

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments