The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp timeseries Command

Syntax:

mdsp timeseries

Help:

mdsp timeseries --help

Alternative form:

mc timeseries

(The CLI was using mc as default command name in older versions)

Description

list timeseries data *

Usage

Parameter list:

Usage: mdsp timeseries|ts [options]

list timeseries data *

Options:
 -i, --assetid Insights Hub asset id
 -n, --aspectname Insights Hub aspect name
 -f, --from begining of the time range to read (default: "2022-11-05T01:51:16.182Z")
 -t, --to end of the time range to read (default: "2022-11-06T01:51:16.182Z")
 -s, --select comma separated list of variable names
 -d, --download download timeseries to a set of files
 -a, --all include also quality codes not just variable values
 -r, --raw don't strip the nextRecord URLs from downloaded JSON
 -h, --formatted write JSON strings with indentation
 -l, --local use local time in timeseries list
 -c, --count number of timeseries entries per request (default: "2000")
 -p, --passkey passkey
 -y, --retry retry attempts before giving up (default: "3")
 -v, --verbose verbose output
 --help display help for command

Examples

Here are some examples of how to use the mdsp timeseries command:

 Examples:

 mdsp timeseries --asssetid 1234567..ef --aspectname Environment list recent timeseries for aspect Environment
 mdsp timeseries --asssetid 1234567..ef --aspectname Environment --select Temperature 
 list recent temperature timeseries 
 mdsp timeseries --asssetid 1234567..ef --aspectname Environment --select Temperature --all 
 list all recent temperature timeseries
 mdsp timeseries --asssetid 1234567..ef --aspectname Environment --select Temperature --all 
 list all recent temperature timeseries
 mdsp timeseries --asssetid 1234567..ef --aspectname Environment --download 
 download the recent timeseries data for the Environment aspect

 Important:

 Please use bulk commands if you want to download a lot of data.

See Insights Hub API documentation for more information about Insights Hub APIs.