The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp upload-timeseries Command

Syntax:

mdsp upload-timeseries

Help:

mdsp upload-timeseries --help

Alternative form:

mc upload-timeseries

(The CLI was using mc as default command name in older versions)

Description

parse .csv file with timeseriesdata and upload the timeseries data to Insights Hub

Usage

Parameter list:

Usage: mdsp upload-timeseries|uts [options]

parse .csv file with timeseriesdata and upload the timeseries data to Insights Hub

Options:
 -c, --config config file with agent configuration (default: "agentconfig.json")
 -r, --cert [privatekey] required for agents with RSA_3072 profile. create with: openssl genrsa -out private.key 3072
 -f, --file csv file containing the timeseries data to upload to Insights Hub
 -s, --size max records per http post (default: "200")
 -n, --no-validation switch validation off (only if you are sure that the timeseries upload works)
 -y, --retry retry attempts before giving up (default: "3")
 -v, --verbose verbose output
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp upload-timeseries command:

 Examples:

 mdsp ts -f timeseries.csv upload timeseries from the csv file to Insights Hub 
 mdsp upload-timeseries --file timeseries.csv --size 100 use http post size of 100 records 

 Data Format: (use your own data point ids from Insights Hub)

 timestamp, dataPointId, qualityCode, value
 2022-11-06T01:51:14.192Z, DP-Temperature ,0, 20.34
 2022-11-06T01:51:15.192Z, DP-Humidity, 0, 70
 2022-11-06T01:51:16.192Z, DP-Pressure, 0, 1012.3

 Make sure that the timestamp is in ISO format. The headers and the casing (timestamp, dataPointId) are important.
 The values must correspond with data types configured in Insights Hub (in example: DP-Humidity must be an integer)

 Important:

 You have to configure the data source and data mappings in Insights Hub asset manager before you can upload the data
 See also: https://documentation.mindsphere.io/resources/html/asset-manager/en-US/116404525451.html

See Insights Hub API documentation for more information about Insights Hub APIs.