The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

TypeScript SDK - Authentication & Authorization

The typescript SDK works with so called Authorizers which can be passed to the constructor of the client. The SDK comes with five authorizer implementations which support different deployment scenarios for your application.

All authorizer implement the TokenRotation interface so that you can also develop your own custom authorizer class by implementing that interface.

Info

The HttpAction method is overridden in different authorizers, this is how the SDK works in both backend and frontend scenarios.

All backend authorizer are automatically rotating the bearer tokens, you don't have to do it manually. For the frontend authorization we suggest to implement some kind of keep alive functionality in your app to avoid session expiration.

export interface TokenRotation {
    RenewToken(): Promise<boolean>;
    GetToken(): Promise<string>;
    GetGateway(): string;
    GetTenant(): string;
    HttpAction(....)}

BrowserAuth

Info

The BrowserAuth authentication and authorization only works for applications which are registered behind Insights Hub APP Gateway

This Authorizer implements support for calling applications from frontend, where Authorization: Bearer... token is not required. Instead, the authorizer reuses the SESSION and XSRF-TOKEN Cookies and sets the X-XSRF-TOKEN header for you.

The Authorizer uses Insights Hub Frontend API Calling Schema:

{web_app_host}/api/

This means that it is using relative URLs as it is expecting to run in the browser behind the Insights Hub API gateway so it will call e.g. /api/identitymanagement/v3/Users instead of https://gateway.eu1.mindsphere.io/api/identitymanagement/v3/Users.

You can simplify your local development by using the Insights Hub development proxy when using this authorizer. You need to redirect the /api/** calls of your application to use the the development proxy which is running on http://localhost:7707.

Code Sample

// Browser authentication is the Default Authentication for the MindSphereSdk
// it is used automatically if no other authorizer is passed
const sdk = new MindSphereSdk();
// this is equivalent to new MindSphereSdk(new BrowserAuth());

const assetManagement = sdk.GetAssetManagementClient();
await assetManagement.GetAssets();

The clients can also be instantiated separately (the MindSphereSdk class is just a convenience.)

const assetManagement = new AssetManagementClient();
await assetManagement.GetAssets();

UserAuth

Info

The UserAuth authentication and authorization only works for applications which are registered behind Insights Hub APP Gatewa

This Authorizer implements support for calling applications from backend, where Authorization: Bearer... Token is required.

The Authorizer uses Insights Hub Backend API Calling Schema:

gateway.{region}.{mindsphere-domain}/api/...

You can simplify your local development by using the Insights Hub development proxy when using this authorizer, just replace the gateway url with http://localhost:7707 when instantiating this authorizer.

Code Sample

Here is the class definition

export class UserAuth extends MindConnectBase implements TokenRotation {
/**
 * Creates an instance of UserAuth.
 * extract token from http request headers (req.get("authorization"))
 *
 * @param {string} token
 * @param {string} gateway
 *
 * extract token from curreny http request:
 * Gateway has to follow the https://gateway.{region}.{mindsphere-domain} schema
 *
 * @see https://developer.mindsphere.io/concepts/concept-authentication.html#calling-apis-from-backend
 *
 * @memberOf UserAuth
 */
constructor(token: string, gateway: string)
}

And here is an example

const bearerToken = request.get("Authorization");

const sdk = new MindSphereSdk(new UserAuth(bearerToken, "https://gateway.eu1.mindsphere.io"));
const identity = sdk.GetIdentityManagementClient();

const newUser = await identity.PostUser({ userName: username });

TokenManager Auth

Info

The UserAuth authentication and authorization only works for applications which are registered behind Insights Hub APP Gatewa and for self hosted applications which are just calling Insights Hub APIs.

This Authorizer implements the bearer token rotation for app credentials.

The Authorizer uses Insights Hub Backend API Calling Schema:

gateway.{region}.{mindsphere-domain}/api/...

If you are using this type of credentials you can call Insights Hub APIs directly, there is no need to use development proxy.

Code Sample

Here is the class definition

export class TokenManagerAuth extends AuthBase implements TokenRotation {

/**
 * Creates an instance of TokenManagerAuth.
 * @param {string} _gateway
 * @param {string} _basicAuth
 * @param {string} _hostTenant
 * @param {string} _userTenant
 * @param {string} _appName
 * @param {string} _appVersion
 * @memberOf TokenManagerAuth
 */
constructor(
    protected _gateway: string,
    protected _basicAuth: string,
    protected _hostTenant: string,
    protected _userTenant: string,
    protected _appName: string,
    protected _appVersion: string
);

The most important part is that you need to build the basic auth token using your Token Manager Login and Password.

Encode the following combination of user name/ID and password/secret using Base64:

<client_id>:<client_secret>

Build the Basic Auth token using the word Basic, followed by a space and the encoding result, e.g.:

Basic ZGlvcDEtaGVybWlvbmUtaGVybWlvbmU6c2RqaGZhc2RqaGZqYXNkaGZqa2FzZGh
const basicAuth = `Basic ${Buffer.from("<yourclientid>" + ":" + "<your_secret>").toString("base64")}`;

const sdk = new MindSphereSdk( new TokenManagerAuth(
        "https://gateway.eu1.mindsphere.io",
        basicAuth,
        "hostTenant",
        "userTenant",
        "myApp",
        "1.0.0"
));
const timeSeries = sdk.GetTimeSeriesClient();
await timeSeries.PutTimeSeries(assetid, aspectname, [{_time: new Date() rpm: "120"}] )

CredentialAuth (deprecated)

You can (almost always) just use TokenManagerAuth instead.

Info

The CredentialsAuth authentication and authorization only works for applications which are registered behind Insights Hub APP Gatewa and for self hosted applications which are just calling Insights Hub APIs.

This Authorizer implements the bearer token rotation for app credentials.

The Authorizer uses Insights Hub Backend API Calling Schema:

gateway.{region}.{mindsphere-domain}/api/...

If you are using this type of credentials you can call Insights Hub APIs directly, there is no need to use development proxy.

Code Sample

Here is the class definition

export class CredentialAuth extends AuthBase implements TokenRotation {

/**
 * Creates an instance of CredentialAuth.
 * @param {string} _gateway
 * @param {string} _basicAuth
 * @param {string} _tenant
 *
 * @memberOf CredentialAuth
 */
constructor(protected _gateway: string, protected _basicAuth: string, protected _tenant: string)

The most important part is that you need to build the basic auth token using your Token Manager Login and Password.

Encode the following combination of user name/ID and password/secret using Base64:

<client_id>:<client_secret>

Build the Basic Auth token using the word Basic, followed by a space and the encoding result, e.g.:

Basic ZGlvcDEtaGVybWlvbmUtaGVybWlvbmU6c2RqaGZhc2RqaGZqYXNkaGZqa2FzZGh

Example Using ServiceCredentials

const basicAuth = `Basic ${Buffer.from("<yourclientid>" + ":" + "<your_secret>").toString("base64")}`;

const sdk = new MindSphereSdk(new CredentialAuth("https://gateway.eu1.mindsphere.io", basicAuth, "hostTenant"));

const timeSeries = sdk.GetTimeSeriesClient();
await timeSeries.PutTimeSeries(assetid, aspectname, [
    { _time: new Date(), rpm: "120", humidity: "12", temperature: "12.5" },
]);

Insights Hub Agent as Authorizer

The Insights Hub agents implement the same TokenRotation interface like all other Authorizers which means that they can be used with SDK as well. (The agents will have a limited set of scopes but important AssetManagement methods will work)

const configuration = require("agentconfig.json");
const agent = new MindConnectAgent(configuration);
agent.SetupAgentCertificate(fs.readFileSync("private.key"));
await agent.OnBoard();

const sdk = new MindSphereSdk(agent);
await sdk.GetAssetManagementClient().GetAssetType(assetTypeId, { exploded: true });

Using credentials instead of Authorizer

For TokenManagerAuth and CredentialAuth you can also use just the object with authentication credentials instead of the Authorizer class.

The following two lines are equivalent:

const sdk = MindSphereSdk(new CredentialAuth("https://gateway.eu1.mindsphere.io", basicAuth, "hostTenant"));
const sdk = MindSphereSdk({ gateway: "https://gateway.eu1.mindsphere.io", basicAuth: basicAuth, tenant: "hostTenant" });

and the same is valid for these lines:

const sdk = new MindSphereSdk(
    new TokenManagerAuth("https://gateway.eu1.mindsphere.io", basicAuth, "hostTenant", "userTenant", "myApp", "1.0.0")
);

const sdk = new MindSphereSdk({
    gateway: "https://gateway.eu1.mindsphere.io",
    basicAuth: basicAuth,
    tenant: "hostTenant",
    usertenant: "userTenant",
    appName: "myApp",
    appVersion: "1.0.0",
});