The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

TypeScript SDK - HttpAction

If a method is missing you can still call Insights Hub APIs using the HttpAction Method which is available on every Client.

Take a look first at this implementation. You should always pass this.GetGateway(), and await this.GetToken() to the HttpAction, which makes sure that the authorizer works correctly.

export class TimeSeriesAggregateClient extends SdkClient {
    // base Url from OpenAPI specification
    private _baseUrl: string = "/api/iottsaggregates/v3";

    // the path parameters belong in the function parameters and the querystring parameters in params object
    public async GetAggregates(
        entityid: string,
        propertyset: string,
        params: { from: Date; to: Date; intervalValue: number; intervalUnit: string; select?: string }
    ): Promise<TimeSeriesAggregateModels.Aggregates> {
        const qs = toQueryString(params);
        return (await this.HttpAction({
            verb: "GET",
            gateway: this.GetGateway(), // always use this.GetGateway()  and this.GetToken()
            authorization: await this.GetToken(), //this is overriden in different authorizers
            //and ensures that the Client works in frontend and in backend.
            baseUrl: `${this._baseUrl}/aggregates/${entityid}/${propertyset}?${qs}`,
            message: "GetTimeSeriesAggregates", // this is used for logging
        })) as TimeSeriesAggregateModels.Aggregates; // always cast to the real result type from models
    }
}

The full HttpAction method has more parameters, here is an explanation for the not so obvious ones:

  • octetStream: indicates that the response is an octetStream (file)
  • multiPartFormData: lets the method know that the content of message should be multipartFormData instead of JSON.
  • rawResponse=true will return HttpResponse instead of parsed and typed JSON message so that you can parse it on your own
  • returnHeaders=true will just return HttpHeaders of the http action
  • ignoreCodes list of HttpCodes for which the method will not throw an exception
/**
 * perform http action
 *
 * @param {({
 *         verb: "GET" | "POST" | "PATCH" | "PUT" | "DELETE";
 *         gateway: string;
 *         baseUrl: string;
 *         authorization: string;
 *         body?: Object;
 *         message?: string;
 *         octetStream?: boolean;
 *         multiPartFormData?: boolean;
 *         additionalHeaders?: Object;
 *         noResponse?: boolean;
 *         rawResponse?: boolean;
 *         returnHeaders?: boolean;
 *         ignoreCodes?: number[];
 *     })} {
 *         verb,
 *         gateway,
 *         baseUrl,
 *         authorization,
 *         body,
 *         message,
 *         octetStream,
 *         multiPartFormData,
 *         additionalHeaders,
 *         noResponse,
 *         rawResponse,
 *         returnHeaders,
 *         ignoreCodes,
 *     }
 * @returns {Promise<Object>}
 *
 * @memberOf MindConnectBase
 */
public async HttpAction({
    verb,
    gateway,
    baseUrl,
    authorization,
    body,
    message,
    octetStream,
    multiPartFormData,
    additionalHeaders,
    noResponse,
    rawResponse,
    returnHeaders,
    ignoreCodes,
}: {
    verb: "GET" | "POST" | "PATCH" | "PUT" | "DELETE";
    gateway: string;
    baseUrl: string;
    authorization: string;
    body?: Object;
    message?: string;
    octetStream?: boolean;
    multiPartFormData?: boolean;
    additionalHeaders?: Object;
    noResponse?: boolean;
    rawResponse?: boolean;
    returnHeaders?: boolean;
    ignoreCodes?: number[];
}): Promise<Object | undefined>

If you have implemented such method call please consider contributing to the SDK.