The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

MindConnect Node-RED Node - Getting Started

Installing the node

The node is available at the npmjs.org registry and can be installed with help of the following command:

# change to your ~./node-red/ folder
cd ~/.node-red/
npm install @mindconnect/node-red-contrib-mindconnect

Info

  • install to the .node-red folder if you have installed node-red globally
  • install to the userDir directory if you have custom userDir
  • make sure that your nodejs version is relatively current

Node-RED - Manage Palette Installation

You can install the node also via the Manage palette feature in the Node-RED administration UI.

palette

How to use the Node-RED node

Since version 3.9.0 it is possible to completely configure the agent from Node-RED. You will only need the initial Boarding configuration from the Insights Hub UI.

Step 0: Create (at least) one asset and one agent in Insights Hub

  • Create an asset in Asset Manager for your data
  • Create an agent of the type MindConnectLib [core.mclib] and store the agent.

Step 1: Get the initial agent configuration from Insights Hub Asset Manager

You can choose between:

  • RSA_3072 public/private key pair (3072bit) for enhanced security which requires more computing power on the devices and
  • SHARED_SECRET shared key (256bit) for lightweight devices.

If you want to use RSA_3072 you will have to create a 3072bit key for your device, e.g.. with openssl:

openssl genrsa -out private.key 3072

There is no additional configuration required for SHARED_SECRET security profile.

boarding configuration

Step 2: Copy the agent onboarding information (and if necessary the RSA 3072 private key) to the node and deploy the flow

Copy the agent onboarding information and optionally the RSA_3072 private key to the node and deploy the flow.

implementation

Step 3: Press the agent configuration button and select the target asset

The most common agent configuration setup is to have a 1:1 mapping between the Node-RED agent which is delivering the data and your target MindSphere Asset. If this type of configuration is sufficient for your use case you just have to click on the asset to which you want to map the data in the asset list. (you can use the filter asset listbox to quickly find your asset)

implementation

The node will automatically configure all necessary data sources and mapping for you. If you need a more complex setup, just click on the MindSphere Configuration Dialog button which will lead you to the configuration dialog in the Insights Hub, where you can create more complex configurations and mappings.

implementation

Step 4: Create and deploy the flow and send data

You can use the node to send timeseries, bulk timeseries, events and files to Insights Hub. The templates for the input messages are listed below, but you can also just use the Agent Information button which will let you copy the corresponding template to clipboard.

implementation

Send data points

The node requires json objects as input in following format (e.g. from a function node)

const values = [
  { dataPointId: "1000000000", qualityCode: "1", value: "42" },
  { dataPointId: "1000000001", qualityCode: "1", value: "33.7" },
  { dataPointId: "1000000003", qualityCode: "1", value: "45.76" },
];

msg._time = new Date();
msg.payload = values;
return msg;

The node will validate if the data is valid for your agent configuration. his feature can be switched off in the settings but it is not recommended to do so.

Send data points in bulk

The node requires json objects as input in following format (e.g. from a function node if you want to use bulk upload)

const values = [
  {
    timestamp: "2018-11-09T07:46:36.699Z",
    values: [
      { dataPointId: "1000000000", qualityCode: "1", value: "42" },
      { dataPointId: "1000000001", qualityCode: "1", value: "33.7" },
      { dataPointId: "1000000003", qualityCode: "1", value: "45.76" },
    ],
  },
  {
    timestamp: "2018-11-08T07:46:36.699Z",
    values: [
      { dataPointId: "1000000000", qualityCode: "1", value: "12" },
      { dataPointId: "1000000001", qualityCode: "1", value: "13.7" },
      { dataPointId: "1000000003", qualityCode: "1", value: "15.76" },
    ],
  },
];

msg.payload = values;
return msg;

Note: All Insights Hub timestamps must be in the ISO format (use toISOString() function).

Send events

The node requires json objects as input in following format (e.g. from a function node). You can send an event to any asset you have access to in your tenant. Just use the asset id in the entityid.

msg.payload = {
  entityId: "d72262e71ea0470eb9f880176b888938", // optional, use assetid if you want to send event somewhere else :)
  sourceType: "Agent",
  sourceId: "application",
  source: "Meowz",
  severity: 30, // 0-99 : 20:error, 30:warning, 40: information
  description: "Event sent at " + new Date().toISOString(),
  timestamp: new Date().toISOString(),
  additionalproperty1: "123",
  additionalproperty2: "456",
};
return msg;

If you are using the custom events instead of Insights Hub Standard Events please include the following switch in the message.

msg._customEvent = true;

File Upload

The node requires json objects as input in following format (e.g. from a function node). You can upload file to any asset you have access to in your tenant. Just use the asset id in the entityid.

msg.payload = {
  entityId: "d72262e71ea0470eb9f880176b888938", //optional (per default files are uploaded to the agent)
  fileName: "digitaltwin.png", // you can also pass an instance of a Buffer
  fileType: "image/png", //optional, it is automatically determined if there is no fileType specified
  filePath: "images/digitaltwin.png", // required if you are using buffer instead of the file name
  description: "testfile",
};
return msg;

If the experimental chunking feature is on, the files which are larger than 8MB will be uploaded in 8 MB Chunks.

Data Lake File Upload

Precondition for data lake upload is that MindSphere Integrated Data Lake is purchased and write-enabled. The node requires json objects as input in following format (e.g. from a function node).

//
// Preconditions : data-lake is purchased and enabled for writing (see mc data-lake --mode write  CLI command)
//
// Agents can only upload files to a path which is prefixed with their agent id
// The MindConnect Node will apply this prefix automatically to the dataLakeFileUpload Path
// You can pass either a javascript buffer or path to file in the dataLakeFile property for upload
// The subTenantId can be optionally added to the messsage

const dataLakeFileInfo = {
  dataLakeFile: "my/path/to/file.txt",
  dataLakeFilePath: "uploads/file.txt",
};

// Uncomment the next code line if you just want to generate an upload url (in msg._signedUrl)
// without actually uploading the file
// msg._ignorePayload = true;

msg.payload = dataLakeFileInfo;
return msg;

Please note:

  • Agents can only upload files to a path which is prefixed with their agent id
  • The MindConnect Node will apply this prefix automatically to the dataLakeFileUpload Path
  • You can pass either a javascript buffer or path to file in the dataLakeFile property for upload
  • The subTenantId can be optionally added to the message

Reading Asset Information

You can read the data (e.g. static asset variables, or full asset information) from Insights Hub using the following message. This can be used to implement a "digital shadow/digital twin" pattern, where the change in the Insights Hub variables is reflected to the real world asset.

msg.payload = {
  assetId: "{assetId}",
  includeShared: false,
  propertyNames: [],
};

return msg;

You can reduce the number of items in payload by specifying list of properties to include in the message: e.g. propertyNames: ["variables"] or ["location"]

Executing custom functions using Insights Hub javascript/typescript SDK

The node can be used to execute a complex script which uses MindSphere javascript/typescript SDK. The node will create an asyncronous function with one parameter (sdk) and the specified function body and execute it. You can only call the Insights Hub APIs which allow agent authorization.

msg.payload = {
  function: `
const assetManagement = sdk.GetAssetManagementClient();
const asset = await assetManagement.GetAsset('{assetId}');
return asset;
`,
};

return msg;

Error handling in the flows

The node can be configured to retry all Insights Hub operations (1-10 times, with delay of time * 300ms before the next try) If you need more complex flows, the node also returns the

msg._mindsphereStatus; // OK on success othervise error
msg._error; // The timestamped error message

properties which can be used to create more complex flows. (e.g. in the flow below, the unrecoverable errors are written in error.log file and the failed data is stored in backupdata.log file)

errorhandling

JWT Token Generation for SouthBound APIs

The node can be used to generate authentication tokens which you can use to call your own custom southbound APIs. The msg.headers will have a Insights Hub Authorization JWT.

msg._includeMindSphereToken = true;

if you just want to get the token without sending any data to Insights Hub

msg._ignorePayload = true;

Treat tokens as you would any other credentials.

Securing API Endpoints

The corresponding API calls for reading the data source configuration and mappings in Agent Configuration and Agent Information dialog require that the user has:

mindconnect.read

permission. The automatic configuration requires

mindconnect.write

permission.

Troubleshooting

If you have problems with your agent:

  1. Stop the agent.
  2. Move or delete the content of the .mc folder (the json files with configuration and authentication settings).
  3. Offboard the agent.
  4. Create new settings for the mindconnect library.
  5. copy the new settings to the node.

Resetting the agent settings from version 3.7.0

Since version 3.7.0. it is possible to delete the content of the .mc/agentconfig.json file and the agent settings directly from the node.

Press on the "delete local configuration" button on the node, confirm the dialog and redeploy the node.

delete local settings

If you are having problems, it is a good idea to restart the Node-RED runtime completely.

Diagnostic in Insights Hub

If the data is not arriving in your configured asset you should take a look if the data is being dropped in Insights Hub because of a misconfiguration. The agent diagnostic button will lead you directly to the agent diagnostic application in the Insights Hub.

diagnostic

Generating the documentation

You can always generate the current HTML documentation by running the command below.

#this generates a docs/ folder the with full documentation of the library.
npm run doc

Proxy support

Set the http_proxy or HTTP_PROXY environment variable if you need to connect via proxy.

# set http proxy environment variable if you are using e.g. fiddler on the localhost.

export HTTP_PROXY=http://localhost:8888

How to setup development environment

# create a directory ../devnodes
cd ..
mkdir devnodes
cd devnodes
# this registers your development directory with node red
npm link ../node-red-contrib-mindconnect

# after that in you can start developing with
cd ../node-red-contrib-mindconnect

npm run start-dev

# your node red flows will be stored in the ../devnodes directory