The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Insights Hub and Industrial IoT Share llms optimized content

Insights Hub drives smart manufacturing through the industrial Internet of Things. Gain actionable insights with asset and operational data and improve your processes.

Notification for Asset Model Changes

Overview

With subscription-based notification, the 3rd party applications can now integrate subscriptions to topics related to Asset Model. Such applications would be then able to receive notifications when there's a change in Asset Model. Applications can respond with desired actions upon receiving a notification such as using GET aspect by ID API, GET asset type by ID API or GET asset by ID API to fetch more details about the respective asset model object, if required. This feature enables developers to build optimized interactions in the applications and make them performant. Moreover, this improves the user experience for the developers. This mechanism enables customers when to poll the Asset Model data.

The notification will be received on the following changes to Asset Model objects:

Aspect Type

  • Create Aspect Type
  • Update Aspect Type
  • Change description
  • Add variable on aspect type
  • Remove variable from aspect type
  • Rename variable on aspect type
  • Change unit on aspect variable
  • Change default value on static aspect variable
  • Delete Aspect Type

Asset Type

  • Create Asset Type
  • Update Asset Type
  • Change description, image on Asset Type
  • Rename Asset Type
  • Add Asset Type direct variable
  • Rename Asset Type direct variable
  • Change unit on Asset Type direct variable
  • Change default value on Asset Type direct variable
  • Change length on Asset Type direct variable of type STRING
  • Delete Asset Type direct Variable
  • Create Aspect on Asset Type
  • Remove Aspect from Asset Type
  • Rename Aspect on Asset Type
  • Delete Asset Type

Asset

  • Create Asset
  • Update Asset
  • Change asset name, description, and location
  • Change or override the default value of the direct asset type variable
  • Change or override the default value of the static aspect variable
  • Delete Asset
  • Move Asset

To create and publish App for consuming Asset Model notifications, refer to How to Subscribe to notifications for Asset Model change

Limitation

  • The underlying messaging service may bring nomenclature/version changes in the near term; which may need changes and adaption in the customer application.

References

FAQs

  1. What is the notification level in the Asset Model?
    • The notification will be available at the tenant level.
  2. What is the maximum number of asset model resource information per notification?
    • The notification will be real-time on an Asset Model change and will be a single message per action.
  3. Can customers get delayed notification?
    • Yes, in case any Insights Hub component is non-operational.