Opcenter Intelligence Service - API Overview¶
Idea¶
Opcenter Intelligence allows you to access and analyze production-relevant contextualized data from multiple sources. The integration with Insights Hub enables data-driven decision-making based on MES and IoT data.
Opcenter Intelligence API Service can be used to access Opcenter Intelligence data to perform analysis and KPI calculation within the supported Insights Hub services.
Specifically, these APIs provide:
- The list of KPIs defined in Opcenter Intelligence including their configuration data.
- KPI calculation results of:
- A single KPI, with an applied filter.
- A single KPI, with an applied filter and a grouping criterion.
- A single KPI, with an applied filter and a target matrix.
- Multiple KPIs, with an applied filter.
The API Service also provides an alternative way to ingest or delete data in Opcenter Intelligence when the standard ETL-based approach using Opcenter Intelligence Connect Cloud is not feasible. It is particularly useful for scenarios involving Insights Hub. Data must be submitted in a predefined JSON format, and the API supports both standard and custom (extension) entities.
Note
This is only applicable for region Europe 1.
Access¶
For accessing Opcenter Intelligence Service, you need to have the role indicated in Opcenter Intelligence Service API roles and scopes.
A user can only interact with objects within their tenant and subtenants.
Prerequisites¶
The following prerequisites are required and common to all APIs:
- The Opcenter Intelligence app is enabled for the tenant.
- The Opcenter Intelligence app is configured, the Opcenter Intelligence environment is deployed and data ingested.
- In Opcenter Intelligence, a smart view is created, deployed, and configured with the necessary measures and attributes.
- Multiple KPIs are created.
Features¶
Opcenter Intelligence APIs provide access to data stored in the Opcenter Intelligence Manufacturing Data Warehouse. For a detailed list of available entities, refer to the Opcenter Intelligence reference manual on the support center.
These APIs also support key operations, including:
- Retrieving KPI configurations.
- Calculating a single KPI with an applied filter.
- Calculating a single KPI with an applied filter and a grouping criterion.
- Calculating a single KPI with an applied filter and a target matrix.
- Calculating multiple KPIs with an applied filter.
Info
- For more details on APIs, refer to Opcenter Intelligence reference manual available on the support center.
- For more details on how to create KPIs in Opcenter Intelligence, refer to Opcenter Intelligence user manual available on the support center.
- The LoadEntitySchema.txt file, available for download from the support center, contains the JSON schemas for all entities.
Limitations¶
The following are the limitations of Opcenter Intelligence API:
- When executing a query, note that the API supports data filtering and provides a mechanism for paginated access. By default, a query returns a maximum of 1000 records.
- The API is accessible from UI and server to server.
- Data can be accessed by custom applications and standard tools via REST/OData APIs that are compatible with IAM/Cognito authentication.
- Query results are cached for 2 minutes.
- Key and Value in the query string must be URL-encoded.
Related links¶
For more information, refer to the following:
- Opcenter Intelligence Concepts
- Opcenter Intelligence documentation is available to customers who sign in to Support Center with Insights Hub / Siemens ID credentials.