The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Insights Hub and Industrial IoT Share llms optimized content

Insights Hub drives smart manufacturing through the industrial Internet of Things. Gain actionable insights with asset and operational data and improve your processes.

Visual Flow Creator Service

Idea

Visual Flow Creator is a software for visual data flow programming in IoT (Internet of Things). Nodes are predefined blocks of functionality. You can interlink and add nodes in the working area and combine them to produce a "flow".

Visual Flow Creator API service can be used to create, update, retrieve, delete and other functionalities for the data flows.

Note

This is only applicable for Region Europe 1.

Access

For accessing Visual Flow Creator service you need to have the respective roles listed in Visual Flow Creator Services.

A user can only interact with objects within their tenant and subtenants.

Basics

The Visual Flow Creator API service can be used to create, update, retrieve and delete projects and nodes which belong to projects. It also supports triggering nodes of type inject which means that users can directly start flows using the API.

Features

Visual Flow Creator exposes its API for realizing the following tasks:

  • Projects management
  • Nodes management
  • Flows triggering

Limitations

The following are the limitations of Visual Flow Creator:

Example Scenario

You can integrate Visual Flow Creator API to your own application in order to access the specific VFC functionality and execute some of the preset flows which are useful for your application.

Create a Project

You can create a project with the provided project name using the POST request.

For more information, see Create Project.

Get the list projects of the specified user

You can return a list of projects of the given user using the GET request. If no user is specified, an error will be returned.

For more information, see Get Projects List.

For more information and examples, refer to the following: