The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Insights Hub and Industrial IoT Share llms optimized content

Insights Hub drives smart manufacturing through the industrial Internet of Things. Gain actionable insights with asset and operational data and improve your processes.

Job Manager Service

Idea

The Job Manager Service allows customers to execute analytical and data science models, which consist of arbitrary paragraphs of code. Currently, the Job Manager Service only supports Apache Zeppelin virtual notebooks.

Info

The Job Manager Service is currently only available in region Europe 1.

Access

For accessing this service you need to have the respective roles listed in Job Manager roles and scopes.

Basics

The Job Manager Service follows an execution pattern, which consists of the following steps:

  1. Validate input parameters, their existence and security availability.
  2. Start the execution environment.
  3. Prepare input data.
  4. Execute Zeppelin virtual notebook.
  5. Store results in user defined output directory.

Dependencies

Model Management Service

The Job Manager Service uses the API of the Model Management Service to access the analytical models to be executed. The respective models must be accessible by the tenant.

Data Exchange Service

The Job Manager Service uses the API of the Data Exchange Service to read input data and export output data. The respective locations must be accessible by the tenant.

Predictive Learning Services

The Job Manager Services runs the specified jobs in a virtual environment. This environment must be defined using the Predictive Learning services.

Apache Zeppelin

Apache Zeppelin is a virtual notebook environment. Apache Zeppelin notebooks support various interpreters, for many languages and frameworks, including Scala, Python, Java etc. They are useful in at least two general scenarios:

  • training a model to obtain an inference model
  • performing inference or prediction tasks

Features

Training a model usually requires high computation resources like memory, storage, bandwidth and CPU. The Job Manager Service exposes its API for realizing the following tasks:

  • Validate provided input before proceeding with expensive operations
  • Perform necessary cleanups regardless of the success or failure of the execution
  • Retry expensive operations automatically in case of failure
  • Record important outputs for the user to backtrace errors
  • Minimize the usage of expensive resources

Limitations

  • All input files have to pass the Gateway, which has its own limitations.

  • Each execution is started in a separate execution environment.

  • Setting up the execution environment can take up to 30 minutes. Keep this in mind for time-sensitive prediction or inference tasks.
  • The preparation time for input data and results is linearly dependent on the file sizes.

API Rate Limits for P&P Tenant

Job Manager has imposed technical limits for P&P tenant to safeguard the system and to avoid system exploitation on heavy load exceeding system limits.API rate limits for Job Manager are applicable as technical rate limits.

Example Scenario

A developer wants to train an Apache Zeppelin notebook model for anomaly detection. The developer uses the Job Manager Service to (re)train this model.