The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Insights Hub and Industrial IoT Share llms optimized content

Insights Hub drives smart manufacturing through the industrial Internet of Things. Gain actionable insights with asset and operational data and improve your processes.

Agent Management Async API

Idea

Agent Management Async API defines topics and message structures to request agent access tokens. The agent access token enables MQTT agents to perform other RESTful operations such as getting asset types, aspect types, large file upload, and writing to IDL. For further information about the Agent Management Async API, refer to the Agent Management Async API specification.

Info

The Agent Management Async API is currently available in region Europe 1.

Access

For accessing these APIs, you need to upload your CA Certificate. For more information, refer Managing CA Certificates.

The agent platforms using this API must support MQTT.

Basics

Agent Access Token Scopes

Agent Access token has the role mdsp:core:DefaultAgent which has the scopes listed in Agent Access Token roles and scopes.

Features

The Agent Management exposes its Async API to MQTT agents for realizing the following tasks:

  • Request agent access token.
  • Receive the result of an agent access token request.

Limitations

  • There are frequency limits per environment and per client for published and received messages.
  • Agent Access Token is valid for one hour. After its expiration, agents need to acquire a new agent access token to continue using Industrial IoT services.

Example Scenario

The MQTT agent needs to exchange large data files with Insights Hub. Sending this through the MQTT broker increases the load for active messages as well as imposes a limitation on the size of the file. The broker and the protocol itself have message limits that are far lower than some use cases. This can be reduced by allowing the agents to directly access the MindConnect API.