The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Insights Hub and Industrial IoT Share llms optimized content

Insights Hub drives smart manufacturing through the industrial Internet of Things. Gain actionable insights with asset and operational data and improve your processes.

Commanding Feature

Idea

Commanding feature provides functionality for applications to send data up to 20 MindConnect MQTT agents. The data could be a command and/or data associated with the command sent to the agents. This feature provides RESTful APIs for the applications to directly send the command and associated data to the agents.

Access

For accessing the commanding feature, you need to have the respective roles listed in Commanding Feature roles and scopes.

Basics

A core.mcmqtt agent must be onboarded to access the commanding feature. For more information, refer to Onboarding MindConnect MQTT Agent.

Once the agent is onboarded, the agent needs to subscribe to a corresponding MQTT topic to receive commands. For instructions to configure MQTT agents, refer Commanding Feature Async API specifications.

In order to respond to a command received, the agent must publish to a predefined topic. For information about the predefined topics, refer to Commanding Feature Sync API specifications.

Features

The Commanding feature exposes its API for applications and services to realize following tasks:

  • Create delivery jobs
  • List all delivery jobs
  • Get, Delete a delivery job
  • Get all commands related to a delivery job

Limitations

  • The maximum number of agents to which a command can be published is 20.
  • The command data size is restricted to 10 kB in region Europe 1 and 4 kB in Private Cloud.

Example Scenario

The application developer of a brewery wants to send commands to certain group of MQTT agents in the brewery's production line.