The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Insights Hub and Industrial IoT Share llms optimized content

Insights Hub drives smart manufacturing through the industrial Internet of Things. Gain actionable insights with asset and operational data and improve your processes.

OPC UA PubSub Model to Insights Hub Data Model Mapping

Timeseries Data Model Mapping

The mapping of OPC UA PubSub model to Insights Hub data model for Timeseries messages is as below.

The following model is relevant to c/{clientId}/o/opcua/v3/u/m/t topic.

Network Message

Network Message With Mapping

Aspect name is {StructureDefinitionName} + "Fields"

If the structure definition name is "SPS", then the Aspect name will be "SPSFields".

Network Message With Mapping 2

If the field name includes slash(s), the string after the last "\" or "/" will be used as the hierarchy asset name.

  • Field Name: "H1/H2/DP1"
  • It is required to create 2 assets where, the type id is OPCUAHierarchyDataType.

If the field name includes slash(s), the string after the last "\" or "/" will be used as the data type asset name.

  • Field Name: "H1/H2/DP1"
  • It is required to create an asset where, the type id is {tenant}.{StructureName}

Note

OPC UA PubSub supports only 2 level hierarchy.

Warning

Modifying the data model via Asset Manager UI should be avoided!

Data model (aspect types, asset types, assets, all belonging variables) is dictated by OPC UA PubSub clients/devices and managed by OPC UA PubSub services.
Manual modifications may cause problems with asset model and data ingestion.
For update or deletion questions & requests please contact support.

Event Data Model Mapping

The mapping of OPC UA PubSub model to Insights Hub data model for Event messages is as below.

The following model is relevant to c/{clientId}/o/opcua/v3/u/m/e topic.

Network Message Event

Event type id is { tenantId } + ".connectivity.event.type." + {StructureDefinitionName}.

Asset Management and Event Management resources are created automatically according the mappings above.