The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Insights Hub and Industrial IoT Share llms optimized content

Insights Hub drives smart manufacturing through the industrial Internet of Things. Gain actionable insights with asset and operational data and improve your processes.

OPC UA PubSub Service Limits and Constraints

General Rules

Publisher

PublisherId in NetworkMessage is used for name field of OPC UA DataModel Asset(core.opcuadatamodel).

Itemfor MindConnect MQTTfor MQTT
Minimum character count116
Maximum character count119128
Allowed characters[a-zA-Z0-9:_-]+[a-zA-Z0-9_~-]+

ClientId will be same with PublisherId for MQTT broker or tenantId_publisherId for MindConnect MQTT.

If all requirements are not met, the entire NetworkMessage will be dropped. For further validations, refer to Asset Management service limitations.

Types

  • StructureDefinition in NetworkMessage is used as AssetType/EventType.
  • KeyValuePairs in NetworkMessage are used as AssetType Variables or Fields of EventType.

StructureField in NetworkMessage is used for Variable of AssetType or Field of EventType.

  • Specific fields such as _time and <variable>_qc are not created as Variable of AssetType.
    • _time is used for timestamp of timeseries.
    • <variable>_qc is used for quality code of specified variable.
  • Specific field such as timestamp is not created as Field of EventType, it exists by default.

For more information, refer Asset Management/Event Management services.

Validation of String Inputs

The maximum length of each string in a NetworkMessage is 255, unless any other specification is informed. If any String value in a NetworkMessage exceeds the maximum limit, the whole NetworkMessage will be dropped.

Specific String Validations

StructureDefinition Name

This field is used for name field of Asset Types/Event Types. For more information, refer Asset Management limitations.

Additional Usage

This field is also additionally used for the name field of Aspect Type in format of <name>Fields.

Aspect Type And Aspect Name

  • Aspect Type Name: Same field of Structure Definition Name is used for "Name" field of Aspect Types. Minimum character count is 1 and maximum character count is 128. Pattern is [a-zA-Z0-9_]+
  • Aspect Name: Same field of Structure Definition Name is used for "Name" field of Aspect. Minimum character count is 1 and maximum character count is 64. Pattern is [a-zA-Z0-9_]+

If it does not meet the requirement, the entire NetworkMessage will be dropped.

Warning

Some additional fields are added while creating Aspect Types, which may cause an error in Asset Management.

Asset Instance

Warning

As OPC UA PubSub specification does not support time zone field, it is not possible to set the time zone field on “Asset”. The time zone field is automatically set as environment's time zone.

StructureField and EnumField Name

  • This field is used for name field of Variables.
  • Minimum character count is 1 and maximum character count is 64. Pattern: [a-zA-Z_][a-zA-Z0-9_]*

If it does not meet the requirement, the entire NetworkMessage will be dropped.

Warning

The validation of the pattern needs to be checked at service level to ensure that it is aligned with the documentation.

FieldMetaData Name

  • This field is used for name field of Assets. Hierarchy asset names are separated by '\' and '/' from this field. Each part after splitting process must meet the below requirements;
  • Minimum character count is 1 and maximum character count is 128. Pattern: [^\/\\]*

If it does not meet the requirement, the entire NetworkMessage will be dropped.

Warning

The validation of the pattern needs to be checked for Hierarchy Asset existence in the name field.

FieldMetaData - Properties Name

  • This field is used for Static Variables of Asset Type (e.g. unit, prefix...).
  • Minimum character count is 1 and maximum character count is 64. Pattern: [a-zA-Z_][a-zA-Z0-9_]*

If it does not meet the requirement, the entire NetworkMessage will be dropped.

Warning

The validation of the pattern needs to be checked at service level to ensure that it is aligned with the documentation.

NodeId

  • According to the OPC UA Part6 1.04.17 spec, NodeId field has various encoding values, in which "Four Byte" type is supported.
  • Any other type than "Four Byte", NodeId causes the entire NetworkMessage to be dropped.

StructureFields[]

  • DataType of StructureField must meet the below requirements:
    • Namespace shall be equal to OPC UA Reserved namespace. Other namespaces are considered as EnumDataType by default, and the value is always processed as a "String" value.
    • Value shall be equal to one of limited BuiltinType (Only 1 to 14 is allowed)
  • Some specific names of StructureField have special meaning in Insights Hub, and those are not created as aspect variables.
    • _time name of a StructureField will be used as timestamp of that specific data on IoT.
    • If a name ends with "_qc", for instance "variable_qc", it means that it is a quality code value of "variable".

FieldMetaData[]

  • Maximum of 800 fields are supported in a MetaData.
  • Name

    • Name of this field must be unique within publisher.
    • All characters are allowed including slash (/) and backslash ().
    • Slash and backslash characters represents hierarchy at field name.
    • Field name is split by slash or/and backslash characters.
    • OPC UA Data Type (core.opcuadatatype) assets are created and latest part of the fields' name is used for asset name.
    • OPC UA Hierarchy Type assets are created for hierarchy parts of the field name.
    • Field name cannot start and end with slash or backslash.
    • Field name Regex: ^[^\\\/][\\\/]{0,1}[^\\\/]$
    • Maximum characters count is 128 for all field name parts.
    • Field name includes maximum of 2 hierarchy assets (3 level).

    Example:

    • Field name: hierarchyPart1/hierarchyPart2/dataFieldName
    • Created Assets:

      hierarchyPart1 : OPC UA Hierarchy Type
          hierarchyPart2 : OPC UA Hierarchy Type
          dataFieldName : OPC UA Data Type
      

EnumDataTypes

  • EnumDataTypes can be encoded by the system, but their values are not used. Instead, if any structureField of a structuredDataType uses custom NodeId values, it will be considered as Enum data type and it is always processed as a "STRING" value.

Properties

  • Even though properties are additional attributes of FieldMetaData objects, they are considered as additional attributes of StructureDescription objects. If a new asset type is going to be created based on StructureDescription, the system will search to find a first FieldMetaData object that contains Properties. The values of the properties will be used as variables of asset type that is going to be created.
    • For example, A StructureDescription describes a custom object type as "SPS". A FieldMetaData describes a custom object instance as "SPS1" with properties as "unit" and "prefix.". These two values will be used in creating a new asset type named "SPS". This means that all other SPS custom object instances are subjected to this structure.
  • The maximum limit of possible value of properties is limited to only two values.

ChunkedNetworkMessagePayload

  • Chunk bundle identifiers are: PublisherId, DataSetWriterId and MessageSequenceNumber.
  • If any chunk message has different totalSize value than other chunk messages, the chunked NetworkMessage will be dropped.
  • If all chunk bundles are not completed, after one day all uploaded chunk bundles are dropped.
  • Maximum number of chunks of a chunkset cannot exceed 20.

Limitations

OPC UA PubSub Limits

ItemSoft Limit
Max number of Publisher per TenantAccording to your agent quota but not more than 100
Max number of DataSetWriterId per Publisher3
Max number of ConfigurationVersion per DataSetWriterId1
Max size of NetworkMessage20KB
Max size of Chunk NetworkMessage20KB
Max size of Chunk bundle200 KB
Max number of of Chunk NetworkMessage30
Max duration time of Chunk packages1 hour

TimeSeries Meta Package (per environment)

ItemSoft Limit
Max number of meta packages per min1
Max size of meta packages200KB
Max number of StructureDefinition25
Max number of Field per MetaData30
Max number of StructureDefinition Field Count50
Total max number of Field per Publisher50
Max number of KeyValuePairs128
Max number of hierarchy level3

TimeSeries Data Package (per environment)

ItemSoft Limit
Max number of data packages per sec1
Max size of data packages200KB

Event Meta Package (per environment)

ItemSoft Limit
Max number of meta packages per min1
Max size of meta packages200KB
Max number of StructureDefinition10
Max number of Field per MetaData50
Total max number ofField per Publisher50
Max number of hierarchy level3

Event Data Package (per environment)

ItemSoft Limit
Max number of data packages per sec1
Max size of data packages200KB