The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Insights Hub and Industrial IoT Share llms optimized content

Insights Hub drives smart manufacturing through the industrial Internet of Things. Gain actionable insights with asset and operational data and improve your processes.

IoT Time Series Aggregates Service – Request Parameters

Ideal Interval Length

Performance Entity

For best performance, choose an interval length which is an exact multiple of a pre-calculated aggregation interval, such as 10 minutes, 2 hours, 5 days, 3 weeks, or 2 months. Requests for other interval lengths take longer to process, because they require using raw time series and pre-calculated aggregations to calculate results.

Simulation Entity

Such entities support only the following intervals - 1ms,10ms and 1s.

Start Time Precision

The requested start and end times cannot be defined with higher precision than the requested interval length. The total time range must be a multiple of the requested interval length. For example, assume a request for data aggregated into intervals of 5 minutes. There, the start time must be defined with minute precision and the total time range must be a multiple of 5 minutes. When requesting data aggregated into intervals of 10 seconds, the start time must be set with second precision and the total time range must be a multiple of 10 seconds.

Interval Precision

The supported interval lengths overlap, which provides flexibility to the application. For example, 1 hour and 60 minutes represent the same length, but allow different behavior. A request for aggregation intervals of 1 hour can only be used for time ranges which start and end at the top of the hour, like 5:00 – 10:00. In contrast, a request for aggregation intervals of 60 minutes can also be used for time ranges like 5:30 – 10:30, which would otherwise be rejected. Accordingly, if the environment is configured with the first day of the week being Monday, a time range of 1 week must start and end on a Monday. A time range of 7 days could start on any day of the week. For more information refer to the Samples.

Parameter Selection

There is an optional select parameter that defines which data to return. For more information, refer to the Selecting documentation.