The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Insights Hub and Industrial IoT Share llms optimized content

Insights Hub drives smart manufacturing through the industrial Internet of Things. Gain actionable insights with asset and operational data and improve your processes.

IoT Time Series Client for Java

Introduction

The IoT Time Series Java client allows you to interact with time series data related to assets. Refer to IoT Time Series for more information about the service.

Hint

In the IoT context, assets are referred to as entity and aspects as propertyset.

Time Series Operations

Client Name: TimeseriesClient

Read latest Time Series Data

Read the latest value of time series data for a single entity and property set.

// Construct the TimeseriesClient object
TimeseriesClient timeseriesClient = TimeseriesClient.builder()
                                        .mindsphereCredentials(credentials)
                                        .restClientConfig(config)
                                        .build();

TimeseriesData timeseriesData = null;
try {
    timeseriesData = timeseriesClient.getLatestTimeseries(entity, propertySetName);
} catch (MindsphereException e) {
    // Exception handling
}

Read Time Series Data

This operation invokes the IoT Time Series API to:

  • Read time series data for a single entity and property set.
  • Return data for a specified time range.
  • Return the latest value, if no range is provided.
  • Return time series data for selected fields and limit.
//Construct TimeseriesClient object as shown above
List<TimeseriesData> timeseriesDataList = null;
try {
    timeseriesDataList = timeseriesClient.getTimeseries(entity, propertySetName, from, to, limit, select);
} catch (MindsphereException e) {
    // Exception handling
}

Write Time Series Data

Write the time series for a single entity and property set. The existing time series data will be overwritten.

Note

The maximum size of a write payload is 1 MB.

//Construct TimeseriesClient object as shown above

boolean success = false;
try {
    success = timeseriesClient.putTimeSeries(entity, propertySetName, timeSeriesList, sync);
} catch (MindsphereException e) {
    // Exception handling
}

Import Time Series Data

Import or update time series for a single entity and property set. The existing time series data is overwritten.

//Construct TimeseriesClient object as shown above

boolean success = false;
try {
    success = timeseriesClient.importTimeseries(entity, propertySetName, timeseriesFile, sync);
} catch (MindsphereException e) {
    // Exception handling
}

Delete Time Series Data

Delete time series entity and property set within a given time range. It also deletes data for all properties within a property set.

Note

Only data of up to 6 months can be deleted at once.

//Construct TimeseriesClient object as shown above

boolean success = false;
try {
    success = timeseriesClient.deleteTimeSeries(entity, propertySetName, from, to, sync);
} catch (MindsphereException e) {
    // Exception handling
}

Page Iterators

The page iterator for the IoT Time Series API client, TimeseriesPageIterator can be used to get a specific page, the next page or the previous page of data.

The page iterators currently support the following operations:

  • getPage(Integer pageNumber);
  • next();
  • previous();

The page iterator instantiation requires an IoT Time Series API client, an entity, a property set name, a date range (from and to dates) and a page size. If the page size is not provided, it defaults to 2000.

Code sample for the IoT Time Series page iterator instantiation and usage:

try {
    //Create the timeseries client
    TimeseriesClient timeseriesClient =  TimeseriesClient.builder()
                                            .mindsphereCredentials(credentials)
                                            .restClientConfig(config)
                                            .build();
    // Create the timeseries page iterator
    TimeseriesPageIterator timeseriesPageIterator =
        new TimeseriesPageIterator(timeseriesClient, entityId, propertySetName, fromDateString, toDateString, pageSize);

    List<TimeseriesData> timseriesDataList = timeseriesPageIterator.getPage(10);
} catch (MindsphereException e) {
    // Exception handling
}