Insights Hub Monitor Plugin SDK – Demo Plugin¶
The distribution files provide a fully working sample for the Insights Hub Monitor Plugin in the demo folder.
The sample demonstrates the basic functionality of the plugin interface and can be enhanced with custom functionality for your own application. This section describes how to get the sample plugin running.
Prerequisites¶
- Source code editor, e.g., Visual Studio Code.
- Developer plan.
- Node.js and npm are installed and configured.
- You have at least the role
mdsp:core:Developerin your tenant.
Building the Plugin¶
- Unzip the SDK and open the
demodirectory in your IDE. Install the SDK using the following command (use the version provided with the sources):
npm install ../src/ihm-plugin-sdk-3.0.1.tgzInstall all other public dependencies:
npm installOpen the
manifest.ymlfile and customize the plugin name.Build the demo plugin using:
npm run build
Configuring the Plugin via the Developer Cockpit¶
Plugin configuration in the Developer Cockpit is very similar to application configuration.
- Open the Developer Cockpit from the Launchpad and select the Dashboard tab.
- Click on Create new application.
- Select the type Insights Hub Monitor Plugin and infrastructure Self Hosted.

- Enter a display name, an internal name and a version number.
- Upload an icon for your plugin
(Support in Operations Insight will come later.) In
Componentstab:- Enter the component name as in the manifest file
- Enter the URL of your plugin.
Usecf app {pluginName}to get the URL for your deployed plugin. - Add one endpoint for the component using
/**to match all paths.
In
Configurationtab:- Adapt the content security policy if required:
default-src 'self' static.eu1.mindsphere.io; style-src * 'unsafe-inline'; script-src 'self' 'unsafe-inline' static.eu1.mindsphere.io; img-src * data:;Configure the plugin settings as you want. Please note, that the json must be valid.
- For a sidebar plugin you can use as example:
{"views":[{"container":"appBar.explore","displayName":{"default":"Sidebar Plugin","en":"Sidebar Plugin"},"icon":"demo","id":"demo.home","navigationMode":"default","type":"default","url":"/"}]}- For an asset plugin you can use as example:
{"views":[{"container":"appBar.explore.assets","displayName":{"default":"Asset Plugin","en":"Asset Plugin"},"icon":"demo","id":"demo.home","navigationMode":"default","type":"default","url":"/"}]}
Click on Save.
If your plugin requires additional scopes, you can configure that in the Role Configuration. 
For this demo plugin you can directly proceed with step 9.
- Register the plugin.
Accept the dialog to assign the roles to your user.
If you configured specific scopes, you have to logout and login again, to get them active.
Open Operations Insight
Depending on you plugin settings, it will be visible
Congratulations!
You have deployed and configured your first Insights Hub Monitor Plugin. You can now prepare your plugin for productive use in the same way as an application.