The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Insights Hub and Industrial IoT Share llms optimized content

Insights Hub drives smart manufacturing through the industrial Internet of Things. Gain actionable insights with asset and operational data and improve your processes.

Insights Hub Monitor Plugin SDK – FAQ

Why does npm install output errors?

Why is the plugin not displayed in Operations Insight?

  • The plugin has not been created with type Insights Hub Monitor Plugin
  • The required role is not assigned to your user.
  • You have not logged out and logged back in after assigning the role to your user.
  • The plugin is not provisioned for this tenant.
  • The plugin configuration is invalid.

Why is the plugin shown on the Launchpad?

  • The plugin has been registered in the Developer Cockpit as a normal app instead of as Insights Hub Monitor Plugin.

Why don't I have the permission to access Insights Hub and Industrial IoT APIs?

  • The required roles have not been assigned to the plugin in the Developer Cockpit.

Why can't I load libraries like bootstrap in my plugin?

  • The CSP header has not been customized in the Developer Cockpit.

How do I remove the plugin from my tenant?

  • Remove the plugin roles from your user (selected users only).
  • Remove it via the Operator Cockpit (all users of the tenant).

Why do I get a pop-up to re-authenticate my session for the plugin?

Insights Hub Monitor- re-authenticate session

  • The Insights Hub Monitor Plugin SDK is not integrated properly.
  • The plugin does not send any requests to the Insights Hub and Industrial IoT backend and therefore the plugin session expired.
    • Click on the button to re-authenticate your session for the plugin in an extra tab and reload Operations Insight afterwards.
    • Refresh the app token automatically, by periodically sending a ping to a Insights Hub backend service (don't forget to add the required roles), e.g.:

      setInterval(refreshToken, 60000);
      
      function refreshToken() {
          var xhr = new XMLHttpRequest();
          xhr.open('GET', 'api/assetmanagement/v3/assets?size=1', true);
          xhr.send();
      }
      

I used the Fleet Manager Plugin SDK in the past. How can I upgrade to use the Insights Hub Monitor Plugin SDK?

The Insights Hub Monitor Plugin SDK is fully compatible. All interfaces and functionality known from the Fleet Manager Plugin SDK is also available now.

  • Replace the mindsphere-fm-plugin-sdk_{version}.tgz in your project with the latest ihm-plugin-sdk_{version}.tgz
  • Run npm i or npm i ihm-plugin-sdk_{version}.tgzdepending on where you saved the sources.
  • Rename in your sources the variables fmProxy and fmPluginBootstrapper to ihmProxy and ihmPluginBootstrapper.
  • Build your plugin and deploy it.
  • Register it in Developer Cockpit as Insights Hub Monitor Plugin.