The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Insights Hub and Industrial IoT Share llms optimized content

Insights Hub drives smart manufacturing through the industrial Internet of Things. Gain actionable insights with asset and operational data and improve your processes.

Integrating MindConnect Library (MCL) to Sony Spresense Environment

Copying MCL to Spresense SDK

  • After cloning Spresense repository as told Development environment, a new folder named "mcl" should be created in "spresense/externals".

  • Copy "mcl_core" and "mcl_connectivity" folders into the new folder "spresense/externals/mcl".

Add Kconfig, LibIncludes.mk, Library.mk Make.defs files

In "spresense/externals/mcl" folder, we need these four files (Kconfig, LibIncludes.mk, Library.mk and Make.defs).

Kconfig

For mcl_core and mcl_connectivity modules, this sample Kconfig can be used.

menu "MindConnect Library"

config EXTERNALS_MINDCONNECT_LIBRARY_CORE
    bool "MCL Core Component"
    default n
    select LIBC_FLOATINGPOINT
    ---help---
        Enable MindConnect Library Core component.

config EXTERNALS_MINDCONNECT_LIBRARY_CONNECTIVITY
    bool "MCL Connectivity Component"
    default n
    depends on EXTERNALS_MINDCONNECT_LIBRARY_CORE
    ---help---
        Enable MindConnect Library Connectivity component.

endmenu # MindConnect Library

LibIncludes.mk

For mcl_core and mcl_connectivity modules, this sample LibIncludes.mk can be used.

ifeq ($(CONFIG_EXTERNALS_MINDCONNECT_LIBRARY_CORE),y)
CFLAGS   += ${shell $(INCDIR) $(INCDIROPT) "$(CC)" "$(SDKDIR)/../externals/mcl/mcl_core/include"}
CXXFLAGS += ${shell $(INCDIR) $(INCDIROPT) "$(CC)" "$(SDKDIR)/../externals/mcl/mcl_core/include"}
CFLAGS += -DMCL_STATICLIB=1
CXXFLAGS += -DMCL_STATICLIB=1
endif

ifeq ($(CONFIG_EXTERNALS_MINDCONNECT_LIBRARY_CONNECTIVITY),y)
CFLAGS   += ${shell $(INCDIR) $(INCDIROPT) "$(CC)" "$(SDKDIR)/../externals/mcl/mcl_connectivity/include"}
CXXFLAGS += ${shell $(INCDIR) $(INCDIROPT) "$(CC)" "$(SDKDIR)/../externals/mcl/mcl_connectivity/include"}
endif

Library.mk

For mcl_core and mcl_connectivity modules, this sample Library.mk can be used.

ifeq ($(CONFIG_EXTERNALS_MINDCONNECT_LIBRARY_CORE),y)
  EXTRA_LIBPATHS += -L "$(EXTLIBDIR)$(DELIM)mcl$(DELIM)mcl_core$(DELIM)src"
  EXTRA_LIBS     += -lmcl_core
endif

ifeq ($(CONFIG_EXTERNALS_MINDCONNECT_LIBRARY_CONNECTIVITY),y)
  EXTRA_LIBPATHS += -L "$(EXTLIBDIR)$(DELIM)mcl$(DELIM)mcl_connectivity$(DELIM)src"
  EXTRA_LIBS     += -lmcl_connectivity
endif

Make.defs

For mcl_core and mcl_connectivity modules, this sample Make.defs can be used.

ifeq ($(CONFIG_EXTERNALS_MINDCONNECT_LIBRARY_CORE),y)
CONFIGURED_APPS += mcl/mcl_core/src
endif

ifeq ($(CONFIG_EXTERNALS_MINDCONNECT_LIBRARY_CONNECTIVITY),y)
CONFIGURED_APPS += mcl/mcl_connectivity/src
endif

Kconfig file in spresense/externals folder

If these directory structure changes are applied before setting up the Spresense development environment, this Kconfig file (which is autogenerated) should contain the line:

source "/<Path for spresense>/externals/mcl/Kconfig"

Otherwise, this line should be added manually.

Add Makefiles

Makefile for mcl_core

Makefile for mcl_core should be placed in "spresense/externals/mcl/mcl_core/src". Here is the sample Makefile for mcl_core module:

-include $(TOPDIR)/Make.defs
-include $(SDKDIR)/Make.defs

BIN = libmcl_core$(LIBEXT)

MCL_CORE_DIR = $(EXTERNAL_DIR)$(DELIM)mcl$(DELIM)mcl_core

CSRCS =  $(wildcard *.c)
CSRCS += ..$(DELIM)lib$(DELIM)cJSON$(DELIM)cJSON.c
CSRCS += http_client$(DELIM)basic$(DELIM)http_client_basic.c
CSRCS += http_client$(DELIM)basic$(DELIM)mbedtls$(DELIM)tls_socket_mbedtls.c
CSRCS += memory$(DELIM)standard$(DELIM)memory.c
CSRCS += crypto$(DELIM)mbedtls$(DELIM)security_mbedtls.c
CSRCS += file_util$(DELIM)standard$(DELIM)file_util.c

VPATH += :..$(DELIM)lib
VPATH += :memory$(DELIM)standard
VPATH += :http_client$(DELIM)basic
VPATH += :http_client$(DELIM)basic$(DELIM)mbedtls

ROOTDEPPATH += --dep-path .
ROOTDEPPATH += --dep-path ..$(DELIM)lib
ROOTDEPPATH += --dep-path memory$(DELIM)standard
ROOTDEPPATH += --dep-path http_client$(DELIM)basic
ROOTDEPPATH += --dep-path http_client$(DELIM)basic$(DELIM)mbedtls

ifeq ($(WINTOOL),y)
CFLAGS += -I"${shell cygpath -w $(MCL_CORE_DIR)$(DELIM)lib}"
else
CFLAGS += -I$(MCL_CORE_DIR)$(DELIM)lib
endif

include $(APPDIR)/Application.mk

Makefile for mcl_connectivity

Makefile for mcl_connectivity should be placed in "spresense/externals/mcl/mcl_connectivity/src". Here is the sample Makefile for mcl_connectivity module:

-include $(TOPDIR)/Make.defs
-include $(SDKDIR)/Make.defs

BIN = libmcl_connectivity$(LIBEXT)

CSRCS =  $(wildcard *.c)

ROOTDEPPATH = --dep-path .

include $(APPDIR)/Application.mk

mbedTLS Network Module

By default MBEDTLS_NET_C is defined and mbedTLS will use its own network module (implemented in net_sockets.c). You may choose to disable it in the configuration header file of mbedTLS and implement your own mbedtls_net_init, mbedtls_net_connect, mbedtls_net_recv, mbedtls_net_send, mbedtls_net_free functions.