The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Terms of Use and Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Norm MicroService

The NORM Service provides validation and normalization capabilities for a larger set of number systems, such as GTIN, MLFB, SFC, SHS, SSN or TNS, etc. See Numbering systems for a full list of currently supported numbering systems.

REST Service API¶

The service is exposed through the API Gateway in the following environments via an REST API. We provide the OpenAPI documentation for the endpoints as well as Postman collections (e.g. for testing) to get you started in the table below.

EnvironmentEndpoint (via API Gateway) Postman Collection
PRODUCTIONhttps://apim.industry.siemens.cloud/norm/v3/Postman Collection
TEST/QAhttps://apim-test.industry.siemens.cloud/norm/v3/Postman Collection

Setup Postman environments and collection¶

Postman is an API(application programming interface) development tool which helps to build, test and modify APIs. You can download Postman from here.

After downloading the Postman files, open Postman, click on Collection and click on Import to import the files.

Click on the name of the imported file like in the picture below, open the Variables tab and enter the client_id and client_secret for the respective environment (DEV, TEST, PROD) in both Initial Value and Current Value columns. Don't forget to click on the Save button

Now open the Authorization tab, scroll down and click on the Get New Access Token button. A pop-up window will come out showing the access token. Click on Use Token.

Now, you are successfully authenticated. You can now send requests and use the NORM-Service.

You can click on Body tab and enter product number to be sent to NORM-Service.