The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Terms of Use and Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Norm MicroService

The NORM Service provides validation and normalization capabilities for a larger set of number systems, such as GTIN, MLFB, SFC, SHS, SSN or TNS, etc. See Numbering systems for a full list of currently supported numbering systems.

Error and Warning Codes¶

Overview¶

NBSystemDescription
4MLFBMLFB contains 9 or/and Z in position seven or higher, but the required short code (ANA) is missing or wrong
5MLFBMLFB has appended -Z, but the required short code (ANN) is missing
8MLFBShort codes shouldn't have more than three positions (ANA / ANN)
9MLFBShort code contains letters I, O or Z
10MLFBShort code ANA is duplicated: {shortcode}
12MLFBThere is no appended -Z despite the presence of short code (ANN)
14MLFBANA shortcode identified but no 9 or Z in position seven or higher
15MLFBFirst position of short code (ANA) is not one of the letters G, H, J, K, L, M, N, P, Q, or R
90MLFBShort code should have Y either in the first position (for ANN) or in the last position (ANA)
91MLFBShort code adapted
101GTINGTIN must be 12, 13 or 14 digits long
102GTINbad checksum {X}. {Y} expected

Examples¶

NBSystemDescriptionExampleMessage Type
4MLFBMLFB contains 9 or/and Z in position seven or higher, but the required short code (ANA) is missing or wrong1ab1234-5z-za23ERROR
5MLFBMLFB has appended -Z, but the required short code (ANN) is missing1ab1234-5z-zj2kERROR
8MLFBShort codes shouldn't have more than three positions (ANA / ANN)1ab1234-5z-zj2krERROR
9MLFBShort code contains letters I, O or Z1ab1234-5z-za23j2kzioERROR
10MLFBShort code ANA is duplicated: H2A1LG4313-9AA60-ZH2A+H2A+A23ERROR
12MLFBThere is no appended -Z despite the presence of short code (ANN)1ab1234-zo12ERROR
14MLFBANA shortcode identified but no 9 or Z in position seven or higher1ab12345c-za23+l1xERROR
15MLFBFirst position of short code (ANA) is not one of the letters G, H, J, K, L, M, N, P, Q, or R1LA83152AA6-za01+a01+b01+b1bERROR
90MLFBShort code should have Y either in the first position (for ANN) or in the last position (ANA)1ab1234-zy12WARNING
91MLFBShort code adapted7MF49123DA07-ZC11C12C20L00V04WARNING
101GTINGTIN must be 12, 13 or 14 digits long00380100ERROR
102GTINBad checksum 4. 8 expected0038010000464ERROR