Advanced Configuration¶
Archived documentation
You are reading the documentation for Polarion 2512. The current release is Polarion 2606.
In addition to the com.siemens.polarion.rest.enabled and com.siemens.polarion.rest.swaggerUi.enabled properties that enable REST API and the Swagger UI, the following additional properties let you further customize the Polarion REST API. They are added to the polarion.properties file.
com.siemens.polarion.rest.cors.allowedOrigins¶
This property enables CORS (Cross-Origin Resource Sharing) access to all REST endpoints.
Supported Values¶
(Standard ports - 80 for HTTP, 443 for HTTPS - should be omitted. For example, https://secured.host.name instead of https://secured.host.name:443)
Note
Requests from the same origin that Polarion is running on are always allowed, regardless of the value in this property.
Requests from origin set in
com.siemens.polarion.rest.baseUrlare always allowed, regardless of the value of this property. (If not defined,baseUrlis used as the default value.)For a Cluster deployment, we recommend that you set the property in the shared
polarion.propertiesfile on the cluster machine to ensure that all the nodes use the same setting.
com.siemens.polarion.rest.maxPageSize¶
This property sets the limit for the maximum page size that can be requested by a REST API client.
The default value is
100.The absolute maximum page size is
10000. (Setting this property to a number larger than10000has no effect.)
Note
For a Cluster deployment, we recommend that you set the property in the shared polarion.properties file on the cluster machine to ensure that all the nodes use the same setting.
com.siemens.polarion.rest.defaultPageSize¶
This property defines the default number of returned items for REST API endpoints.
If
defaultPageSizeexceeds themaxPageSize(see above), thedefaultPageSizevalue is replaced by themaxPageSizevalue.The default value is
100
com.siemens.polarion.rest.bodySizeLimit¶
This property limits the size of the request body in an HTTP request.
The limit is only valid for HTTP POST, HTTP PATCH, and HTTP DELETE requests with application/json content type.
The value is given as bytes.
Note
This limit also applies to the size of the JSON file that is used when POSTing or PATCHing attachments. Also, using a high value for this property might make the Polarion server vulnerable from a security point of view.
com.siemens.polarion.rest.maxIncludedSize¶
This property specifies the number of results that are returned per page in the Included section for REST API endpoints. For more information, see Limit of included resources.
If the number of entities exceeds the
maxIncludedSize, they are not added to the Included section when requested.The default value of this property is
500items, with a maximum limit of10 000.If the provided value exceeds the
10 000limit, it is capped.
com.siemens.polarion.rest.maxRelationshipSize¶
This property specifies the maximum number of entities that can be returned for each of the resource(s) relationship field(s). For more information, see Limit of included resources.
If the number of entities exceeds the
maxIncludedSize, they are not added to the Included section when requested.The default value of this property is
500items, with a maximum limit of10 000.If the provided value exceeds the
10 000limit, it is capped.