The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Advanced Configuration

In addition to the com.siemens.polarion.rest.enabled and com.siemens.polarion.rest.swaggerUi.enabled properties that enable REST API and the Swagger UI, the following additional properties let you further customize the Polarion REST API. They are added to the polarion.properties file.

com.siemens.polarion.rest.cors.allowedOrigins

This property enables CORS (Cross-Origin Resource Sharing) access to all REST endpoints.

Supported Values

  • Empty list Blue arrow CORS is disabled.

  • * Blue arrow CORS requests from any host are allowed.

  • Comma separated list of URI (schema://host:port) Blue arrow Only CORS requests from these origins are allowed.

(Standard ports - 80 for HTTP, 443 for HTTPS - should be omitted. For example, https://secured.host.name instead of https://secured.host.name:443)

Note

  • Requests from the same origin that Polarion is running on are always allowed, regardless of the value in this property.

  • Requests from origin set in com.siemens.polarion.rest.baseUrl are always allowed, regardless of the value of this property. (If not defined, baseUrl is used as the default value.)

  • For a Cluster deployment, we recommend that you set the property in the shared polarion.properties file on the cluster machine to ensure that all the nodes use the same setting.

com.siemens.polarion.rest.maxPageSize

This property sets the limit for the maximum page size that can be requested by a REST API client.

  • The default value is 100.

  • The absolute maximum page size is 10000. (Setting this property to a number larger than 10000 has no effect.)

Note

For a Cluster deployment, we recommend that you set the property in the shared polarion.properties file on the cluster machine to ensure that all the nodes use the same setting.

com.siemens.polarion.rest.defaultPageSize

This property defines the default number of returned items for REST API endpoints.

  • If defaultPageSize exceeds the maxPageSize (see above), the defaultPageSize value is replaced by the maxPageSize value.

  • The default value is 100

com.siemens.polarion.rest.bodySizeLimit

This property limits the size of the request body in an HTTP request.

The limit is only valid for HTTP POST, HTTP PATCH, and HTTP DELETE requests with application/json content type.

The value is given as bytes.

Note

This limit also applies to the size of the JSON file that is used when POSTing or PATCHing attachments. Also, using a high value for this property might make the Polarion server vulnerable from a security point of view.

com.siemens.polarion.rest.maxIncludedSize

This property specifies the number of results that are returned per page in the Included section for REST API endpoints. For more information, see Limit of included resources.

  • If the number of entities exceeds the maxIncludedSize, they are not added to the Included section when requested.

  • The default value of this property is 500 items, with a maximum limit of 10 000.

  • If the provided value exceeds the 10 000 limit, it is capped.

com.siemens.polarion.rest.maxRelationshipSize

This property specifies the maximum number of entities that can be returned for each of the resource(s) relationship field(s). For more information, see Limit of included resources.

  • If the number of entities exceeds the maxIncludedSize, they are not added to the Included section when requested.

  • The default value of this property is 500 items, with a maximum limit of 10 000.

  • If the provided value exceeds the 10 000 limit, it is capped.