The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Changelog

0.3.2 (2026-07-06)

✨ Features

  • Added support for wstring ROS data type

0.3.1 (2026-03-12)

💥 Breaking Changes

  • Renaming from ROSie to ROXSIE

✨ Features

  • Added support for comments and constants defined in ROS .msg files
  • Added support for SIMATIC Open Controller 3
  • Added RMW installation parameter to build_deploy_container.sh for generated ROS 2 workspace
  • Added command line message to refer to generated log file in case of a generation error

🔌 API Changes

  • Renaming of headers from rosie_api to roxsie_api
  • Renaming of namespace from ROSie to ROXSIE
  • Renaming of ROS 2 node from ROSieNode to ROXSIENode
  • Renaming of client variable from _rosie_client to _roxsie_client

🐛 Bug Fixes

  • Adapted installation script to handle empty user inputs
  • Carriage return characters will be filtered out from ROS 2 .msg definitions
  • Added IEC check for all generated SCL code blocks in TIA Portal
  • Fixed generation failure for copying custom interface packages to generated ROS 2 workspace

0.3.0 (2025-09-05)

✨ Features

  • Added support for RIB v2.2.4
  • Increased usability by automatically creating a complete ROS 2 workspace including the generated ROS 2 package (with all custom interface packages if defined) and docker deploy files
  • Added video tutorial and engineering system guide sections to documentation for more user friendly setup and usage descriptions
  • Modified docker build scripts to give the user more control for specifying the ROS 2 version and container name for their generated ROS 2 package
  • Renamed generated input directory to yaml_input within output folder
  • Added automatic search for ROS 2 Jazzy and other custom ROS 2 installations within the ROSie installer script
  • Improved code generation error handling by providing additional information via .log file in the generated environment directory

🔌 API Changes

  • Changed ROSie API header file rosie.hpp to provide a non-copyable ROSie client class, as objects should not be copied because of possible shared memory issues
  • Adapted ROSie API header file rosie_return_value.hpp return type to be of type struct ReturnValue instead of std::pair<ReturnCode, std::string> for more readable return value handling

0.2.0 (2025-05-08)

✨ Features

  • Added support for ROS 2 Jazzy
  • Some changes in the generated .scl code file (e.g. valid elements counter prefix to i_valid_elements_*) to not violate the TIA style guide
  • Added GIF's to documentation for more user friendly setup and usage descriptions

0.1.1 (2024-11-15)

✨ Features

  • Removed deprecated optional PLC arguments (cyclic_interrupt_ob_name, read_db_name, write_db_name) from YAML config
  • Switched to HTML-based interactive user documentation (not yet released)
  • Improved runtime performance on PLC side for topics not containing strings
  • Improved installation process
  • Updated generator base docker image
  • Improved error messages when user provided a non-compliant YAML config file
  • Added checks for maximum allowed topic rate
  • Updated log messages
  • Added deployment application example for generated ROS 2 packages based on docker
  • Added checks for topic names
  • Added checks for maximum memory usage
  • Added checks for limit of OBs and RIB DBs
  • Fixed issue with failed generation process (missing header rosidl_typesupport_cpp/macros.h) if user provides standard ROS 2 installation instead of a source build
  • Various bugfixes and performance improvements of the generator

0.1.0 (2024-08-30)

✨ Features

  • First functional Minimum Viable Product (MVP) release based on RIB v2.1.1 and ROS 2 Humble
  • Includes support for ROS 2 publishers & subscribers with all standard and custom message types