The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Limitations

String Size

The RIB only supports fixed size arrays of bytes to store string like texts.
Therefore, ROS 2 message types that contain strings e.g. string frame_id in std_msgs/msg/Header will translate those strings to a fixed size byte array with the size of 254 bytes (as shown in the picture below).
⚠️ As the byte array will be available as a string on the PLC side, it is also converted on the PLC side. The PLC based string data type defines the maximum string length of 254 bytes.

Max String Size

WString Size

The RIB currently supports fixed size arrays of uint16 to store wide strings.
Therefore, ROS 2 message types that contain wide strings (e.g., wstring) will translate those strings to a fixed size array of RIB_UINT16. The default length is 254 WChars (similar to regular strings). In contrast to regular strings, the maximum wide string length can be configured up to 4096 WChars.
⚠️ As the RIB_UINT16 array will be available as a WString on the PLC side, it is also converted accordingly. The type conversion from uint16 to WString on the PLC side is time consuming (~ 3 times higher than standard String type), therefore the usage of wide strings should be avoided at higher frequencies (>100 Hz) and only be used with caution.

Vector Size

As the RIB does not provide dynamic SHM allocation during runtime, all ROS 2 based vector types are currently limited to a fixed size of 64 elements.
⚠️ Additionally, a valid elements counter variable will be added to the PLC side, so that the user can define, how many valid elements are stored in the vector, if the number is smaller than 64.

Max Vector Size

Shared Memory

As the RIB uses shared memory to access data through Industrial OS as well as the Software Controller (SW-PLC),
The actual size of the used shared memory area is therefore limited and has to be conform to the memory limit of the SW-PLC.

Max SHM Description

An example usage is shown in the picture above, where the two ROS 2 message types geometry_msgs/msg/Twist and sensor_msgs/msg/BatteryState are used to provide data to the PLC (ros2_to_plc) via shared memory.

Those two definitions are combined to one shared memory area during runtime, that shall not exceed the actual SW-PLC memory limitations:

SW-PLC
Type
v30.1
Code memory limit [MB]
v31.1
Code memory limit [MB]
v40.0
Code memory limit [MB]
S7-1505 SP223
S7-1505 SP F224.5
S7-1505 SP T (F)334.5
S7-1507 S (F)55—
S7-1508 S (F)1010—
S7-1508 T (F)12.512.5—

⚠️ Note: As those limitations are defining the total PLC code memory limit, the used ROS 2 .msg typse that needs to be transfered to the PLC or vice versa should not be too big regarding memory layout.

Number of RIB Clients

The RIB and its participant manager RIB_App supports up to 128 client applications.
But as the generated ROS 2 package uses a precompiled RIB API library, currently only one ROS 2 client connection is possible, combined with one SW-PLC based connection.

Max RIB Clients

Number of Data Blocks / Symbols

The SW-PLC supports in total up to 20 Cyclic Interrupt Organization Blocks (OBs).
As each topic in the YAML configuration defines one Cyclic Interrupt OB (ROS 2 -> PLC and vice versa), the user needs to make sure that the provided YAML defines less than 20 topics in total or up to 16 topics for each side (ROS 2 -> PLC and vice versa) as shown in the picture below.

Max Data Blocks

⚠️ The user has to keep in mind that the defined topics and therefore Cyclic Interrupt OBs will be added to already existing ones.

Additionally, the RIB provides the following maximum specifications:

RIBMax. number of symbols (topics)Max. number of provide / consume DBs
v2.1.1102416
v2.2.481921024

Comments

ROS 2 .msg files may contain comments using the # character.
ROXSIE carries these comments over into the generated SCL code, if they follow one of the two supported syntaxes:

Inline comment: A # directly after a variable definition on the same line, followed by the comment text:

float32 voltage          # Voltage in Volts (Mandatory)

Continuation comment: A line consisting only of leading whitespace followed by #, continuing the comment of the variable + comment defined on the previous line:

float32[] cell_voltage   # An array of individual cell voltages for each cell in the pack
                         # If individual voltages unknown but number of cells known set each to NaN

Both styles are demonstrated in the ROS 2 standard interface package: sensor_msgs/msg/BatteryState.msg.

⚠️ Comments that do not follow either of the above formats — for example, standalone comment blocks not attached to a variable, or continuation lines missing the required leading whitespace — will not be included in the generated SCL code.

Constants

ROS 2 .msg files support the definition of typed constants by assigning a fixed value to a named identifier using the = sign.
ROXSIE recognizes these constant definitions and generates corresponding constant declarations in the generated SCL code.

A ROS constant follows the syntax <type> <NAME> = <value>, optionally followed by an inline comment:

uint8 POWER_SUPPLY_TECHNOLOGY_UNKNOWN = 0 # Unknown battery technology
uint8 POWER_SUPPLY_TECHNOLOGY_NIMH = 1    # Nickel-Metal Hydride battery

By convention, constant names are written in UPPER_SNAKE_CASE to distinguish them from regular variable definitions.
Inline comments on constant lines are carried over into the generated SCL code using the same rules as described in the Comments section above.

Full examples of constant definitions can be found in the ROS 2 standard interface package: sensor_msgs/msg/BatteryState.msg.

⚠️ Constants are read-only values and will not be mapped to any RIB shared memory — they are purely informational declarations available on the PLC side.

Topic Rates

At this stage, the RIB connections provided in the YAML config should not exceed a specified rate of 1000 Hz.
⚠️ The jitter for a defined rate highly depends on the complexity of the provided data type. For example, a geometry_msgs/msg/Twist is able to reach a stable rate of 1 kHz, but a more complex data type such as trajectory_msgs/msg/MultiDOFJointTrajectory with its vector of strings and nested structs will cause a loss of data at this rate or exceeding the PLC cycle time causing the PLC to stop!
⚠️ The usage of strings and/or wstring and/or vectors and/or nested structs of them should be avoided at higher frequencies (>100 Hz) as their conversion is time consuming!

Generated ROS 2 Package

The generated C++ based ROS 2 package has the following properties:

  • The generated ROXSIE API C++ code is not thread safe (as the RIB connection does not provide thread safe shared memory access).
  • The global RIB cycle time for ROS 2 values written to the RIB will be set to the highest of all topic frequencies defined in the provided YAML config file.
  • The ROXSIE API code is based on the C++17 standard.
  • The ROXSIE generated ROS 2 code is only tested with Humble and Jazzy.
  • All primitive ROS 2 types are supported.

Type Conversions

The following table shows the available standard data types and their corresponding data types in ROS 2, RIB and TIA.

ROS 2 data typeRIB data typeTIA data typeComment
boolRIB_BOOLBool
byteRIB_BYTEByte
charRIB_BYTEChar
float32RIB_FLOATReal
float64RIB_DOUBLELReal
int8RIB_INT8SInt
int16RIB_INT16Int
int32RIB_INT32DInt
int64RIB_INT64LInt
uint8RIB_UINT8USInt
uint16RIB_UINT16UInt
uint32RIB_UINT32UDInt
uint64RIB_UINT64ULInt
stringRIB_BYTE[254]StringThe maximum string length is currently capped at 254 characters
wstringRIB_UINT16[254]WStringThe maximum wide string length is capped at 4096 WChars (8192 bytes), default is 254 WChars

For arrays the conversion is:

ROS 2 data typeRIB data typeTIA data typeComment
[10][10]Array of [0..9]

For vectors the conversion is:

ROS 2 data typeRIB data typeTIA data typeComment
[][64]Array of [0..63] of Vectors will be converted to arrays of a fixed size (currently storing 64 elements)
RIB_UINT32UDIntAdditionally a i_valid_elements_* variable will be created for each ROS 2 vector on the RIB and TIA side to track the actual elements the ROS 2 vector contains / shall contain

⚠️ Transferring ROS 2 vectors with more elements than the maximum size (current default is 64) will lead to data loss.