The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Requirements

To utilize ROXSIE there are two systems involved:

  1. Engineering System: Used to run the ROXSIE generator (e.g., a Windows engineering machine with Linux as subsystem).
  2. Runtime System: Used to execute the generated code (e.g., a SIMATIC Industrial OS system with RIB and Software PLC).

1. Engineering System Requirements

Engineering System

Hardware

  • Any x86/x64 based system

Software (all of the listed)

  • ROXSIE container running in a Linux environment with access to ROS 2 installation via ENV variables
  • Linux (e.g. SIMATIC Industrial OS, Ubuntu, Debian) + Windows 10/11 (for TIA Portal) operating systems
  • ROS 2 running natively in Linux or in a container if installation is mounted to host to be accessible by ROXSIE container
  • Docker (+ Docker Compose plugin) >= v20.x.y
  • TIA Portal running in Windows 10/11

⚠️ Note: To be able to use the RIB with Software Controller v31.1, TIA Portal v20 >= Update 1 needs to be installed.

The use of virtual machines or Windows Subsystem for Linux (WSL) is recommended in order to have TIA Portal and ROS 2 running in parallel in the same system.
Please refer to the Engineering System Setup for a detailed step by step instruction on how to prepare your engineering system.

2. Runtime System Requirements

Runtime System

Hardware (one of the listed)

DeviceNameShipped
IndOS
Version
Shipped
SW-PLC
Version
Recommendations
OC2SIMATIC ET 200SP Open Controller CPU 1515SP PC2 - (F)v3.x.yv3x.y🔋 Embedded / Low Power
- Ideal for compact installations
- Direct IO modules access
OC3SIMATIC ET 200SP Open Controller CPU 1515SP PC3 - (F)v4.x.yv4x.y🔋 Embedded / Low Power
- Successor to PC2
- Ideal for compact installations
- Direct IO modules access
427ESIMATIC IPC 427Ev3.x.y—
(must be purchased separately)
⚖️ Balanced Performance
- Great compromise between performance and efficiency
BX39ASIMATIC IPC BX-39Av4.x.y—
(must be purchased separately)
⚖️ Balanced Performance
- Successor to 427E
- Great compromise between performance and efficiency

All of the listed devices have been tested and verified to work with ROXSIE generated code.
This list is non-exhaustive and other devices might work with ROXSIE too as long as they fulfil the following software requirements.

Software (all of the listed)

Software Version Compatibilities

The following table shows the supported software versions of all ROXSIE releases:

ROXSIESoftware ControllerTIA PortalIndustrial OSRIBROS 2 (tested)
v0.1.0v30.1v19v3.4.2v2.1.1Humble
v0.1.1v30.1v19v3.4.2v2.1.1Humble
v0.2.0v30.1v19v3.4.2v2.1.1Humble, Jazzy
v0.3.0v30.1, v31.1v19, v20 >= Update 1v3.4.2, v3.5.3v2.1.1, v2.2.4Humble, Jazzy
v0.3.1v30.1, v31.1, v40.0v19, v20 >= Update 1v3.4.2, v3.5.3, v4.2.0v2.1.1, v2.2.4Humble, Jazzy
v0.3.2v30.1, v31.1, v40.0v19, v20 >= Update 1v3.4.2, v3.5.3, v4.2.0v2.1.1, v2.2.4Humble, Jazzy

Additionally, each Software Controller version requires a specific TIA Portal, Industrial OS and RIB version:

Software ControllerTIA PortalIndustrial OSRIB
v30.1v19v3.4.2v2.1.1
v31.1v20 >= Update 1v3.5.3v2.2.4
v40.0v20 >= Update 4v4.2.0v2.2.4