Troubleshooting¶
Environment Variable Errors¶
This kind of error occurs, if the user did not setup the host environment properly e.g. via the setup guideline or manually by setting the host environment variables in the .env file accordingly, e.g. like shown below.
# [REQUIRED]
# The users ROS 2 base installation path share directory that contains all standard interfaces including their .msg files.
# This directory has to be be mounted in the ROXSIE container to be able to lookup all standard types.
# Standard ROS 2 installation example: /opt/ros/jazzy
# Custom ROS 2 installation example: /home/${USER}/jazzy_ws
USER_ROS2_INSTALLATION_PATH=/opt/ros/jazzy
# [OPTIONAL]
# The user directory where the optionally needed custom ROS 2 interfaces are installed.
# Example: /home/user/ros2_ws
USER_ROS2_INTERFACE_INSTALLATION_PATH=/home/user/ros2_ws
# [REQUIRED]
# The current directory where this .env file and the whole provided ROXSIE workspace is located.
# This directory should contain an <input> directory that stores the config.yaml files and an <output> directory where the generated code is stored.
# Example: /home/${USER}/roxsie_workspace
USER_ROXSIE_WORKSPACE_PATH=/home/user/roxsie_workspace
USER_ROXSIE_WORKSPACE_PATH¶
The USER_ROXSIE_WORKSPACE_PATH environment variable defines the path to your actual ROXSIE workspace. Here, the input and output directories as well as the docker-compose.yaml and .env files should be located.
⚠️ Variable Not Defined¶
If you did not define the ROXSIE workspace, where the input/output directories are located, the following error will be displayed:
$ roxsie -c example_config.yaml
#################################### ROXSIE ###################################
# Version: 0.3.2 #
# Date: dd.mm.YYYY #
# Time: HH:MM:SS #
# Copyright (c) Siemens AG, 2026, and licensors. All rights reserved. #
# Portions include Open Source Software. See ReadMe_OSS_0.3.html for details. #
#################################################################################
Environment variable <USER_ROXSIE_WORKSPACE_PATH> is not declared.
A log file with more information was generated in the <output/YYYY_mm_dd_HH-MM-SS/environment>
⚠️ Wrong Workspace¶
If you provided a workspace path, that is not existing, the following error should be displayed:
$ roxsie -c example_config.yaml
#################################### ROXSIE ###################################
# Version: 0.3.2 #
# Date: dd.mm.YYYY #
# Time: HH:MM:SS #
# Copyright (c) Siemens AG, 2026, and licensors. All rights reserved. #
# Portions include Open Source Software. See ReadMe_OSS_0.3.html for details. #
#################################################################################
Environment variable path </home/user/non_existing_path> does not exist.
A log file with more information was generated in the <output/YYYY_mm_dd_HH-MM-SS/environment> directory.
✔️ Possible Solution¶
As a solution, the install script scripts/install_roxsie_environment.sh can be executed, or the environment variable USER_ROXSIE_WORKSPACE_PATH (.env file) can be set manually.
USER_ROS2_INSTALLATION_PATH¶
If you are using standard ROS 2 interface configurations e.g. geometry_msgs/msg/Twist, the USER_ROS2_INSTALLATION_PATH environment variable is crucial for ROXSIE to locate your standard ROS 2 installation directory.
This variable should point to the root directory of the ROS 2 installation, where all .msg and include/lib definitions are located.
⚠️ Variable Not Defined¶
If the USER_ROS2_INSTALLATION_PATH environment variable is not defined, ROXSIE will not be able to find necessary standard ROS 2 message definitions, leading to errors during gathering all data type information.
The following error message will be displayed:
$ roxsie -c example_config.yaml
#################################### ROXSIE ###################################
# Version: 0.3.2 #
# Date: dd.mm.YYYY #
# Time: HH:MM:SS #
# Copyright (c) Siemens AG, 2026, and licensors. All rights reserved. #
# Portions include Open Source Software. See ReadMe_OSS_0.3.html for details. #
#################################################################################
Gathering ROS 2 message types information ...
Environment variable <USER_ROS2_INSTALLATION_PATH> is not declared.
A log file with more information was generated in the <output/YYYY_mm_dd_HH-MM-SS/environment> directory.
⚠️ Wrong ROS 2 Installation Path¶
If the provided USER_ROS2_INSTALLATION_PATH points to a directory, which does not exist, the output should look like the following:
$ roxsie -c example_config.yaml
#################################### ROXSIE ###################################
# Version: 0.3.2 #
# Date: dd.mm.YYYY #
# Time: HH:MM:SS #
# Copyright (c) Siemens AG, 2026, and licensors. All rights reserved. #
# Portions include Open Source Software. See ReadMe_OSS_0.3.html for details. #
#################################################################################
Gathering ROS 2 message types information ...
Environment variable path </home/user/non_existing_ros2_install_path> does not exist.
A log file with more information was generated in the <output/YYYY_mm_dd_HH-MM-SS/environment> directory.
✔️ Possible Solution¶
You can solve those issues by either running the install script scripts/install_roxsie_environment.sh or manually setting the environment variable USER_ROS2_INSTALLATION_PATH.
With the manual step, the USER_ROS2_INSTALLATION_PATH variable needs to point to the correct path of your ROS 2 installation. This can be a standard ROS 2 installation like /opt/ros/jazzy or a source installation such as /home/user/jazzy_ws.
Note that the naming extension .../install is important if you are using a custom ROS 2 installation.
USER_ROS2_INTERFACE_INSTALLATION_PATH¶
In addition to standard ROS 2 message types, you can define and provide custom .msg definitions to ROXSIE.
Therefore, the environment variable USER_ROS2_INTERFACE_INSTALLATION_PATH has to be set to provide the path to your custom ROS 2 interface installation directory e.g. /home/user/ros2_ws.
⚠️ Type Not Found¶
If you defined custom ROS 2 .msg definitions and the USER_ROS2_INTERFACE_INSTALLATION_PATH environment variable is not defined, ROXSIE will not be able to find the corresponding custom ROS 2 message definitions, leading to errors during the gathering of all data type information.
An output like the following will be displayed:
$ roxsie -c custom_config.yaml
#################################### ROXSIE ###################################
# Version: 0.3.2 #
# Date: dd.mm.YYYY #
# Time: HH:MM:SS #
# Copyright (c) Siemens AG, 2026, and licensors. All rights reserved. #
# Portions include Open Source Software. See ReadMe_OSS_0.3.html for details. #
#################################################################################
Gathering ROS 2 message types information ...
Could not find ROS 2 type file <custom_msgs/msg/CustomType.msg>. Make sure the ENV variable <USER_ROS2_INTERFACE_INSTALLATION_PATH> is set if you provided a custom ROS 2 interface in the YAML config.
A log file with more information was generated in the <output/YYYY_mm_dd_HH-MM-SS/environment> directory.
✔️ Possible Solution¶
You can solve those issues by either running the install script scripts/install_roxsie_environment.sh or manually setting the environment variable USER_ROS2_INTERFACE_INSTALLATION_PATH.
Usage Errors¶
As ROXSIE is a command-line tool, errors can occur easily and therefore, the following common errors can occur.
Ownership of start-roxsie Script¶
It could occur that the start-roxsie script in /usr/local/bin has a problem with the ownership when using the binary installer.
$ start-roxsie
/bin/bash: /usr/local/bin/start-roxsie: Permission denied
✔️ Possible Solution¶
You can fix it changing the ownership of the script:
sudo chown $USER:$USER /usr/local/bin/start-roxsie
No Configuration File¶
⚠️ ROXSIE is used with the --config [-c] parameter but without the required YAML configuration file name.
$ roxsie -c
#################################### ROXSIE ###################################
# Version: 0.3.2 #
# Date: dd.mm.YYYY #
# Time: HH:MM:SS #
# Copyright (c) Siemens AG, 2026, and licensors. All rights reserved. #
# Portions include Open Source Software. See ReadMe_OSS_0.3.html for details. #
#################################################################################
Invalid option provided: missing argument for -c
✔️ Provide the exact name of the YAML configuration file that your want to use and which is placed in the input directory of your ROXSIE workspace.
Wrong Configuration File Name¶
⚠️ ROXSIE is used with the --config [-c] parameter and a non-existing YAML configuration file.
$ roxsie -c non_existing_config.yaml
#################################### ROXSIE ###################################
# Version: 0.3.2 #
# Date: dd.mm.YYYY #
# Time: HH:MM:SS #
# Copyright (c) Siemens AG, 2026, and licensors. All rights reserved. #
# Portions include Open Source Software. See ReadMe_OSS_0.3.html for details. #
#################################################################################
YAML configuration file <non_existing_config.yaml> does not exist in workspace input directory.
A log file with more information was generated in the <output/YYYY_mm_dd_HH-MM-SS/environment> directory.
✔️ Provide the name of a YAML configuration file name, which file exists in the ROXSIE workspace input directory.
No PSC File¶
⚠️ ROXSIE is used with a valid YAML configuration file as well as the --psc_file [-t] parameter, but without a corresponding .psc file name.
$ roxsie -c example_config.yaml -t
#################################### ROXSIE ###################################
# Version: 0.3.2 #
# Date: dd.mm.YYYY #
# Time: HH:MM:SS #
# Copyright (c) Siemens AG, 2026, and licensors. All rights reserved. #
# Portions include Open Source Software. See ReadMe_OSS_0.3.html for details. #
#################################################################################
Invalid option provided: missing argument for -t
✔️ Provide a .psc file, that exists in the ROXSIE workspace input directory.
Note that this parameter combination only makes sense with the use of the --non_interactive [-y] flag to go through the whole generation process without user interaction.
Wrong PSC File Name¶
⚠️ ROXSIE is used with a valid non-interactive parameter combination but with providing a .psc file name, that either does not exist in the input directory or is spelled wrong.
$ roxsie -y -c example_config.yaml -t non_existing_project.psc
#################################### ROXSIE ###################################
# Version: 0.3.2 #
# Date: dd.mm.YYYY #
# Time: HH:MM:SS #
# Copyright (c) Siemens AG, 2026, and licensors. All rights reserved. #
# Portions include Open Source Software. See ReadMe_OSS_0.3.html for details. #
#################################################################################
Gathering ROS 2 message types information ...
Generating PLC code ...
TIA project .psc file <non_existing_project.psc> does not exist in workspace input directory.
A log file with more information was generated in the <output/YYYY_mm_dd_HH-MM-SS/environment> directory.
✔️ Provide a .psc file, that exists in the ROXSIE workspace input directory or is spelled correct.
Missing PSC File in Non-Interactive Mode¶
⚠️ ROXSIE is used in non-interactive mode (-y), which requires the .psc file an additional argument.
$ roxsie -c example_config.yaml -y
#################################### ROXSIE ###################################
# Version: 0.3.2 #
# Date: dd.mm.YYYY #
# Time: HH:MM:SS #
# Copyright (c) Siemens AG, 2026, and licensors. All rights reserved. #
# Portions include Open Source Software. See ReadMe_OSS_0.3.html for details. #
#################################################################################
Gathering ROS 2 message types information ...
Generating PLC code ...
The argument --psc_file [t] and .psc file name must be set in non-interactive mode.
A log file with more information was generated in the <output/YYYY_mm_dd_HH-MM-SS/environment> directory.
✔️ Extend the command with the parameter --psc_file or -t plus the name of the .psc file you want to use and which is placed in the ROXSIE workspace input directory.
Wrong PSC File For Provided YAML Configuration¶
⚠️ ROXSIE is used in non-interactive mode with a YAML configuration, that does not match the provided .psc file. Therefore the ROXSIE API code fails to compile.
$ roxsie -y -c project_1.yaml -t project_2.psc
#################################### ROXSIE ###################################
# Version: 0.3.2 #
# Date: dd.mm.YYYY #
# Time: HH:MM:SS #
# Copyright (c) Siemens AG, 2026, and licensors. All rights reserved. #
# Portions include Open Source Software. See ReadMe_OSS_0.3.html for details. #
#################################################################################
Gathering ROS 2 message types information ...
Generating PLC code ...
Generating ROXSIE API library and ROS 2 package ...
Could not generate ROXSIE API code.
A log file with more information was generated in the <output/YYYY_mm_dd_HH-MM-SS/environment> directory.
✔️ Provide a .psc file, that was previously generated with the same YAML configuration based PLC code.
ROXSIE API Code Generation Error¶
⚠️ During the ROS 2 package generation step, the ROXSIE API code generation fails.
$ roxsie -y -c project_1.yaml -t project_1.psc
#################################### ROXSIE ###################################
# Version: 0.3.2 #
# Date: dd.mm.YYYY #
# Time: HH:MM:SS #
# Copyright (c) Siemens AG, 2026, and licensors. All rights reserved. #
# Portions include Open Source Software. See ReadMe_OSS_0.3.html for details. #
#################################################################################
Gathering ROS 2 message types information ...
Generating PLC code ...
Generating ROXSIE API library and ROS 2 package ...
Could not generate ROXSIE API code.
A log file with more information was generated in the <output/YYYY_mm_dd_HH-MM-SS/environment> directory.
✔️ Take a look at the generated <date+timestamp>/environment directory, where a file named <date+timestamp>_extended_roxsie_logs.log provides more detailed information about the actual error.
Please contact us or your Siemens region in case the error can not be solved directly.
FAQ¶
How can I check which RIB version is installed on my IPC?¶
✔️ The actual RIB version can be checked via the RIB_App executable:
RIB_App --version
How can I check which Industrial OS is installed on my IPC?¶
✔️ The Industrial OS version information can be displayed with the following command:
cat /etc/os-release