The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Time and Dates

RFC3339

In the vast majority of APIs, Senseye uses the RFC3339 standard to represent dates and times.

An example of date and time conforming to RFC3339 is: 2022-12-05T13:22:38.000-08:00

For completeness, the RFC3339 specification is here

Formally, the syntax is

   date-fullyear   = 4DIGIT
   date-month      = 2DIGIT  ; 01-12
   date-mday       = 2DIGIT  ; 01-28, 01-29, 01-30, 01-31 based on
                             ; month/year
   time-hour       = 2DIGIT  ; 00-23
   time-minute     = 2DIGIT  ; 00-59
   time-second     = 2DIGIT  ; 00-58, 00-59, 00-60 based on leap second
                             ; rules
   time-secfrac    = "." 1*DIGIT
   time-numoffset  = ("+" / "-") time-hour ":" time-minute
   time-offset     = "Z" / time-numoffset

   partial-time    = time-hour ":" time-minute ":" time-second
                     [time-secfrac]
   full-date       = date-fullyear "-" date-month "-" date-mday
   full-time       = partial-time time-offset

   date-time       = full-date "T" full-time

There are two aspects to draw attention to:

  • the Date format is yyyy-mm-dd i.e. the year, the month and then the day
  • there is a time offset at the end. In the above example, -08:00 is used which represents UTC-8 (Pacific Standard Time). For UTC, +00:00 can be used or Z which stands for the Zero or Zulu timezone (UTC+0).

Senseye stores data in UTC+0 time.

Unix Time

A commonly used lightweight protocol to convey data about a sensor is SenML, which is described here. This standard allows time to be represented as the number of seconds after January 1st, 1970 at UTC.

Unix Time is not used in Senseye's GraphQL API, but is used within the JSON time series data API.