The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Parquet

Apache Parquet is a free and open-source column-oriented data storage format.

Structure

The expected schema for parquet files is as follows:

schema.parquet
assetId: { type: 'UTF8' }
measures: {
    repeated: true,
    fields: {
        name: { type: 'UTF8' }
    }
}
data: {
    repeated: true,
    fields: {
        time: { type: 'UTF8' },
        measureName: { type: 'UTF8' },
        value: { type: 'DOUBLE', optional: true },
        stringValue: { type: 'UTF8', optional: true }
    }
}

The root of schema is an object which contains multiple fields:

  • assetId: a UTF8 string containing a unique mapping ID for a sensor. If a sensor with the mapping ID does not exist, a new sensor will be automatically provisioned.
  • measures: an array of the measure names included within the data array.
  • data: an array of data points. There should be one entry per timestamp.
  • data.time: the timestamp of the entry. Should be a UTF8 string conforming with RFC3339 dates and times, including timezone - more details on the required format are available here.
  • data.measureName: a string name given to the measurement. This value will be the name associated with the time series within Senseye.
  • data.value or data.stringValue: the value of the measure. This can be either a double-precision float number or a string.

File

Name

To avoid file collisions, the name of the file should be unique. To aid debugging, we recommend composing the file name using two components: an ID for the asset being monitored, and a unix timestamp, separated by @ - as an example: motorM23@1651149458.parquet.

Size

Please limit Parquet files to no more than 1MB.

Version

The file must be exactly parquet format version 1.0.

Encoding

The data file must use the parquet binary format and be encoded with one of the following supported codecs:

  • PLAIN
  • RLE

Compression

The supported compression methods are:

  • UNCOMPRESSED
  • GZIP
  • SNAPPY
  • LZO
  • BROTLI