SiGREEN PCF API – API Overview¶
Additional Information regarding the Preview section¶
The API preview is intended to provide a glimpse of the upcoming changes and features in the next version of SiGREEN. Please note that this documentation is subject to change and is not final until the official release of the new SiGREEN version. Users should treat this API preview as a work-in-progress and not rely on it for mission-critical applications or integrations. The official release notes and documentation for the new SiGREEN version should be consulted once available.