The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Smarter Power Distribution. Zero Disruption. Total Visibility. Sm@rtGear® IE is an intelligent power distribution solution designed for the demands of industrial environments with real-time monitoring, predictive diagnostics, and remote-control capabilities.

EV Device

Overall Topic Identification Guide


This Data Point subtopic represents the EV Device data provided by the Sm@rtgear IE DPU (or other polling applications) that are being sent over the databus. In order to subscribe to these data points, the subscription will need the EV Device data category subtopic at the beginning of the topic string, "5".

5/Data Point/Device Type/Device Name/Device Source
flowchart LR
    A[Category: 5] --> B[Data Point - Numeric]
    B --> C[Device Type - Numeric]
    C --> D[Device Name - String]
    D --> E[Device Source - String]

Point Family

Each datapoint is grouped into a broader "family" of other points that measure different aspects of the same thing. This categorization helps in terms of data measurement and understanding the different measurements being taken. Below are all the data point families for EV Device Data subtopic.

flowchart LR
    A[Device Analytics<br>0-16]

Device Analytics

Point Name (Unit)NumberData TypeOverall TopicApp Source(s)Ingested Source(s)Notes
Config0Device Event5/0/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM
Alm Controlled - Current Average1double5/1/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM(V1)Needs to be changed to standardized average current
Percent Utilization (of max charging level)2double5/2/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM
Com Failure3boolean5/3/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM(V1)Needs to be changed to standardized Device Connected
EV Status(1=Pause(blue), 2=ChargingAvailable(green))4boolean5/4/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM
Set Charging Level5double5/5/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM
Alm Controlled - kw6double⅚/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM(V1)Needs to be changed to standardized active power total
Alm Controlled - kVA7double5/7/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM(V1)Needs to be changed to standardized apparent power total
Alm Controlled - kVAr8double⅝/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM(V1)Needs to be changed to standardized reactive power total
Alm Controlled - PF9double5/9/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM(V1)Needs to be changed to standardized reactive power total
Charging Status(true= charging, false=notcharging)10boolean5/10/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM
Reset Command active11boolean5/11/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM
Statistics - Number of reset commands12double5/12/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM
Statistics - Number of pauses13double5/13/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM
Statistics - Number of charging starts14double5/14/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM
Statistics - Operating hours15double5/15/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM
Alarm - Active alarm message16boolean5/16/{DEVICE TYPE}/{DEVICE NAME}/{DEVICE SOURCE}ALM

Back to Top