The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Smarter Power Distribution. Zero Disruption. Total Visibility. Sm@rtGear® IE is an intelligent power distribution solution designed for the demands of industrial environments with real-time monitoring, predictive diagnostics, and remote-control capabilities.

Sm@rtGear® IE System

Purpose

This Data Point Subtopic represents the available system settings provided by the host IED or SG IE system that are being sent over the databus. In order to subscribe to these data points, the subscription will need the Sm@rtGear® IE System category subtopic at the beginning of the topic string,"0".

For example, if an application needs the Sm@rtGear® IE HHeartbeat, they would subscribe to the "0/#" category. If they want to get a specific data point from the category, they would first need to subscribe to the category subtopic, then the data point subtopic (ex. "CAT/DP/#" or "0/0/#" for the Sm@rtGear® IE HHeartbeat).

Point NamePoint Datapoint
SmartGear IE Heartbeat0
CPU Core Count20
CPU Architecture21
CPU Model Name22
CPU Usage Percentage23
CPU Free Usage Percentage24
Free Memory30
Total Memory31
Used Memory32
Used Memory Percentage32
Free Memory Percentage33
Free Storage40
Total Storage41
Used Storage42
Used Storage Percentage43
Correlation ID44