The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Smarter Power Distribution. Zero Disruption. Total Visibility. Sm@rtGear® IE is an intelligent power distribution solution designed for the demands of industrial environments with real-time monitoring, predictive diagnostics, and remote-control capabilities.

Topic Identification

This page gives a comprehensive understanding of our topic structure used for messaging through the MQTT Protocol. It provides explanations and visuals on how to categorize, subscribe to, and manage data points efficiently. This resource is the foundation of understanding our topic model for publishing data.
graph LR;
    A(Sm@rtGear DPU) -- Published with  <br> detailed topic format--> B((MQTT Databus));

Topic Format

Category/Data Point/Device Type/Device Name/Device Source
graph LR;
    A[Category - Numeric] --> B[Data Point - Numeric]
    B --> C[Device Type - Numeric];
    C --> D[Device Name - String];
    D --> E[Device Source - String];

{Category} Numeric: The group type of data being transferred

{Data Point} Numeric: The specific data point being requested

{Device Type} Numeric: The type of device that the data is coming from

{Device Name} String: The specific name of the device that is transferring the data

{Device Source} String: Additional name specification of the device providing the information


Wildcard

When subscribing to a topic, wildcards are used to to subscribe to different subtopics simultaneously within the same topic string. This allow to capture all the data provided by a certain subtopic at different levels.

Single-Level

A single level wildcard can only replace one topic level within a topic string.

graph LR
    A[Category]
    A --> B[Data Point]
    B --> C{{+}}
    C --> D[Device Name]
    D --> E[Device Source]

In this topic string, we are subscribed to all the different {Device Type} information available from the MQTT Databus

Multi-Level

A multi level wildcard can replace multiple topic levels at the end of a topic string.

graph LR
    A[Category]
    A --> B[Data Point]
    B --> C[Device Type]
    C --> D{{#}}

In this topic string, we are subscribed to all the different {Device Name} and {Device Source} information available from the MQTT Databus


Examples

Example 1: Subscribing to Electrical AC Metering Data - Current L1 (refer to Electrical AC Metering Page)

Category Subscription
"11/21" category
- "11" represents the Category
- "21" represents the data point

To get specific data point from the category, subscribe to the category subtopic first, then the data point subtopic.

Data Point Subscription
(ex. "CAT/DP/#" or "11/21/#" for the Current L1).
# - Multi-Level Wildcard
graph LR;
    A[11] --> B[21];
    B --> C{{# :  Device Type/Device Name/Device Source}};

The multi-level (#) represents all the possible subtopics subscribed to simultaneously.


Example 2: Subscribing to Temperature Metering Data - Temperature Reading (refer to Temperature Metering Page)

Category Subscription
"13/1" category
- "13" represents the category
- "1" represents the data point
Data Point Subscription
(ex. "CAT/DP/#" or "13/1/#" for the Temperature Reading).
# - Multi-Level Wildcard
graph LR;
    A[13] --> B[1];
    B --> C{{# :  Device Type/Device Name/Device Source}};

The multi-level (#) represents all the possible subtopics subscribed to simultaneously.


Back to Top