The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Consumption reporting

Vilocify customers buy different sized packages of API requests and component requests (see MLFBs) that are consumed over a time period. We call this time period the consumption period. The ordered packages can't be used after the consumption period ends and unused API requests can't be transferred to the next consumption period. Consumption periods of an organization can't overlap.

During the consumption period Vilocify tracks consumption based on the API requests that organizations and their users make. Admins can see all usage of all members of their organization in the Portal At the end of a consumption period every admin receives an email with a report detailing the usage of the period. The report includes the overall amount of ordered packages and usage details of every membership. Users can see their own consumption and the overall organization consumption on the dashboard, but can't see usage of other users.

When the organization runs out of available requests no user of the organization can perform API requests. This includes usage of the Web Portal, because the portal uses the API. There is no enforcement to restrict a single user, or in other words:

Warning

A single user can consume all requests allocated to an organization

What happens when you run out of requests

When an organization used up all the ordered requests, the API will respond with a 402 error code and almost all features in Web UI will be locked. It's possible to order extensions during a consumption period. Contact your regional Siemens sales person or open a support ticket.

API details

API Details regarding consumption reporting and enforcement are documented in the API documentation.

Available MLFBs

For our external customers, Vilocify can be procured using MLFB order numbers. These are listed for your reference in the following table.

Name of the productMLFBDescription
API V2 - Small9LA1110-1DV14-1AA236000 API requests for 3 memberships in one organization for one year
API V2 - Standard9LA1110-1DV14-1AB2300000 API requests for 50 memberships in one organization for one year
API V2 - Individual*9LA1110-1DV14-1AC2individual offer
API V2 - Extension9LA1110-1DV14-1AD2additional 6000 API requests for the current period (only in combination with Small or Standard)
API V2 - Initial Setup9LA1110-1DV14-2AB2Setup organization and 8 hours of technical support
API V2 - New component9LA1110-1DV14-3AA2Mapping or creation of one new component submitted through a component request

* Please note that individual offers are available upon request.