Skip to content
Siemens Developer Portal

BACnet Health

The Enlighted on-prem Manage (EM) server integrates seamlessly with the Building Management System (BMS) via the BACnet interface. Use this API to poll the Enlighted Manage to determine if BACnet is running or not.

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/bacnet/health

Parameters

Name Description
Request
em_ip_address_or_hostname Manage’s IP address or hostname
Response
status: 0 – BACnet is running; 1 – BACnet not running

Sample Request

Poll the Manage server with the IP address to see if BACnet is running. The response ‘0’ indicates BACnet is running.

GET https://{192.80.3.2}/ems/api/org/bacnet/health

Sample Response

{
  "status": "0"
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments