Skip to content
Siemens Developer Portal

Update Demand Response for Selected Facilities

Update the current running or scheduled Demand Response for a list of selected facilities in the organization for a specific period from the start time.

Request

POST  https://{em_ip_address_or_hostname}/ems/api/org/dr/updatedr/facilities/{facility specification list}
{
    "pricelevel": "LOW",
    "duration": "60",
    "starttime": "2015-07-21T12:15:49+05:30",
    "dridentifier": "DR16",
    "pricing": "15.0"
 }

Parameters

Path Parameters

Request

Name Description
em_ip_address_or_hostname The Manage’s IP address or hostname
facility specification list Schedules a demand response for a list of selected facilities. List of facilities separated by commas. Each facility contains facility type and facility ID: {facility type}_{facility ID}.
Facility Type: Can be either a company, campus, building, or floor. Facility ID: A unique identifier that is assigned to the company or organization, campus, building or floor. (Facility ID is returned in Get All Floors API).
Note: Specifying a facility other than the floor automatically assigns DR to all floors under the facility. Assigning a campus will assign DR to all floors for all buildings on the campus.
For example,
1. To assign DR to the first and second floors of a building, type floor_1,floor_2. DR will be assigned to floor 1 and floor 2.
2. To assign DR to all floors in the Headquarters Building with ID 22, type Building_22. DR will be assigned to all floors in building 22.
pricelevel DR pricing: HIGH / MODERATE / LOW / SPECIAL
duration The DR duration time in minutes (must be a whole number)
starttime Time from when DR should be in effect. Format: (yyyyMMddHHmm) year/month/day/hour/minutes. for example, 15-11-18T17:43:00
dridentifier DR identifier provided at the time of scheduling.
pricing DR pricing that is effective for the energy consumed during the DR period (optional)

Response

Name Description
status 0 – DR schedule successful
1 – DR not scheduled
msg Message description

Sample Request

For example, update the currently running Demand Response (DR) event from LOW to HIGH price level for Floor 1 in Building 51, Campus 1, for 60 minutes starting at 5:30 am on 07-21-2015 at 15 cents. The response indicates that the DR update was successful.

The user must access the web service with proper session/authenticated token:

POST https://192.80.30.2/ems/api/org/dr/updatedr/facilities/floor_1,building_51,campus_1 

Sample Response

{
  "pricelevel": "HIGH",
  "duration": "60",
  "starttime": "2015-07-21T12:15:49+05:30",
  "dridentifier": "DR16",
  "pricing": "15.0"
}

{
  "status": "0",
  "msg": "DR updated successfully"
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments