The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp asset-types Command

Syntax:

mdsp asset-types

Help:

mdsp asset-types --help

Alternative form:

mc asset-types

(The CLI was using mc as default command name in older versions)

Description

list, create or delete asset types *

Usage

Parameter list:

Usage: mdsp asset-types|at [options]

list, create or delete asset types *

Options:
 -m, --mode [list|create|delete|template | info] list | create | delete | template | info (default: "list")
 -f, --file .mdsp.json file with asset type definition
 -i, --idonly list only ids
 -s, --schema JSON Schema
 -n, --assettype the asset type name
 -c, --includeshared include shared asset types
 -k, --passkey passkey
 -y, --retry retry attempts before giving up (default: "3")
 -v, --verbose verbose output
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp asset-types command:

 Examples:

 mdsp asset-types --mode list list all asset types
 mdsp asset-types --mode list --assettype Pump list all asset types which are named Pump
 mdsp asset-types --mode template --assettype Pump 
 create a template file (Enironment.assettype.mdsp.json) for assettype Pump
 mdsp asset-types --mode create --file Pump.assettype.mdsp.json 
 create asset type Pump in Insights Hub

See Insights Hub API documentation for more information about Insights Hub APIs.